January 19, 2022 – AutomationDirect has added more Wiegmann enclosure options to their extensive lineup of over 7,000 modular and pre-fab enclosures. Wiegmann is one of the largest enclosure manufacturers in North America, manufacturing a wide variety of carbon steel, galvanized steel, stainless steel, and aluminum enclosures.
New additions include NEMA 4/4X/12/13 rated stainless steel 22mm pushbutton enclosures, NEMA 4 rated carbon steel wiring troughs with hinged cover, and NEMA 1 rated carbon steel corner-mount wiring troughs, including models with knockouts.
Wiegmann enclosures start at $9.75, with the new wiring troughs starting at $168.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo