February 1, 2023 – AutomationDirect now offers Cat6a industrial Ethernet cables from Murrelektronik. These shielded cables include an M12 X-coded connection on one end and an RJ45 connection on the other.
The X-coded designation is commonly used with industrial vision systems. These high-flex industrial Ethernet cables are available in lengths up to 5m with transmission speed capability up to 10Gbps. These cables have a TPE (thermoplastic elastomer) jacket that is flame-retardant and chemical resistant.
The new Murrelektronik Cat6a Ethernet cables start at $66.00 (3.2ft/1m) and come with a one-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo