March 1, 2023 – AutomationDirect has added new Murrelektronik surge suppression devices that help protect and lengthen the life of motors, contactors, relays, solenoids, and PLC outputs. These new surge suppression devices support a variety of applications and provide protection from voltage spikes and electromagnetic noise caused by inductive loads.
New additions include universal surge suppressors that reduce high voltage spikes created when contactor coils are de-energized, motor surge suppressors that protect 3-phase motors from the damaging effects of line surges, and valve surge suppressors that mount between the valve base and valve plug to protect against damage caused by voltage spikes from solenoid coils.
The new Murrelektronik surge suppressors are CE marked, RoHS compliant, offer a 1-year warranty, and start at $8.00.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo