March 22, 2023 – AutomationDirect has added more FATH hardware components to their selection of T-slotted rail products. These components easily install in SureFrame rails, as well as many other brands, and include roll-in T-slot nuts with spring loaded ball, slide-in T-slot nuts, screw and miter connectors, 1- and 2-slot pivot joints, extended swivel bases, foot consoles, leveling casters, magnetic catches, sensor mounting blocks, protection profiles, profile sliders, roller elements, and much more.
Also added is a 4-axis workstation and workstation components which allow PC monitors and peripherals to be mounted near the equipment. Components include swivel monitor mounts, monitor mounting joints, multi-axis mounting supports, and many other accessories.
New panel holders and panel mounting blocks are also available for wire mesh or solid machine guarding. These holders and mounting blocks allow the installation of machine guarding to protect equipment and personnel from damage and injury.
The new FATH T-slotted rail hardware components start at $2.00 and come with a one-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo