![Photo of custom painted enclosures](https://library.automationdirect.com/wp-content/uploads/2024/05/saginaw-custom-painted-enclosures-launch.jpg)
May 29, 2024 – AutomationDirect now offers custom paint selections for Saginaw carbon steel Enviroline series single-door enclosures with ¼-turn latches. These enclosures can be custom-ordered with one of 15 color options in addition to the standard gray or light gray color. Custom paint options include graphite black, gentian blue, light blue, pebble gray, traffic orange, flame red, zinc yellow, moss green, and more.
Enviroline enclosures are stylish, versatile all-purpose enclosures that feature a flush-fitting door with a flange trough collar around the door opening to channel liquids away. The removable doors are secured by the exclusive SCE concealed hinge that allows a 180-degree opening. The standard 1/4-turn semi-flush latches can be replaced with a variety of specialty latch insert choices.
Enviroline enclosure models offer NEMA 3R, 4, 12 and 13 ratings; stainless steel models also meet NEMA 4X. Custom-painted enclosures are made to order, requiring a setup fee of $233 per color, regardless of quantity.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo