NewsPress ReleasesPress Releases

Wall Lenk Soldering Irons and Guns from AutomationDirect

Wall Lenk soldering irons and guns

July 10, 2024 – AutomationDirect has added Wall Lenk soldering irons and guns designed to join different metals to make a strong and permanent bond. Wall Lenk is a US-based company that has been manufacturing and providing top-quality soldering equipment for over 50 years. The new pencil-style soldering irons are compact and easy to use and include models up to 80 watts in corded versions, and 30 watts in cordless versions, with a variety of interchangeable/exchangeable tip options.

Soldering guns are heavy-duty tools designed for challenging soldering jobs that require demanding heating ranges of up to 400 watts. These soldering guns are available in dual-heat models with 3-position (off/low/high) triggers and a variety of interchangeable/exchangeable tip options.

All soldering tools have polycarbonate impact-resistant bodies with durable stainless-steel shafts and mica-insulated nichrome heating elements.

The new Wall Lenk soldering irons start at $14.50 and soldering guns start at $37.00.

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/

Editorial Contact:         Tina Gable

Phone:                         678-455-1845

Email:                          tgable@automationdirect.com

Download:                   High Resolution Photo