AutomationDirect has added 189 new fiberglass enclosures, subpanels and accessories to its Hubbell-Wiegmann line of non-metallic enclosures.
Starting at $143.00, the new Classic Series of enclosures is designed for general electrical and electronic applications as well as applications requiring broader environmental concerns. The enclosures enhance the appearance of any instrument installation. They are especially suited for high visibility locations found in both industrial and commercial applications, but the chemical resistance and watertight capabilities make them ideal across a broad spectrum of environmental installations as well.
New enclosure models have also been added to the existing Premier, Slim Line, JIC and Control Series lines of Hubbell-Wiegmann fiberglass enclosures.
The Premier Series was developed for design flexibility and pleasing aesthetics.
The Slim Line Series is built around two enclosure designs. Both feature a slim style with flush side walls.
The JIC Series enclosures follow the original design of fiberglass enclosure products featuring a modest overhang cover on a flange mounted base.
The Control Series enclosures are designed to accommodate electrical, electronic, instrumentation and mechanical controls indoors and outdoors where corrosion resistant watertight enclosures are needed to provide protection against windblown dust and rain, splashing and hose directed water.
Learn more by visiting: www.automationdirect.com/enclosures.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
*Prices as of February 22, 2017. Check website for most current prices