New ProductNewsPress ReleasesPress Releases

AutomationDirect Offers Customer Specified Cut-to-Length Cable by the Foot

Bulk multi-conductor industrial automation cable from AutomationDirect is now available in customer specified lengths in one-foot increments from 20 to 5000 ft. Cut-to-length cable eliminates waste and lowers cost (only as much cable as required is purchased).

cable by the footWith a low minimum cut length of 20 feet, the price per foot per cable type is the same regardless of length ordered. There are no cut charges and on orders over $49, there are no shipping charges. Cable is cut to length at AutomationDirect’s own UL Certified respooling facility and is available for same day shipping if ordered by 6:00pm ET.

Cut-to-length multi-conductor cable types include flexible portable cord, RS232/ RS422/ RS485 data cable, flexible control (tray) cable, instrumentation cable, continuous flexing control cable, and continuous flexing industrial Ethernet cable.

Cut-to-length cables start at $0.30 per foot (20-foot minimum), have a one-year warranty and are backed by AutomationDirect’s standard 30-day return policy.

Learn more by visiting: www.automationdirect.com/cut-to-length-cable

To read more press releases from AutomationDirect, click here.

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.

Editorial Contact:              Tina Gable

Phone:                                678-455-1845

Email:                                tgable@automationdirect.com