Issue 57, 2025NewsNotebook IssuePress ReleasesPress Releases

Ardent Multimeters & Accessories from AutomationDirect

July 30, 2025 – AutomationDirect has added Ardent digital multimeters, testers, and testing accessories which are ideal tools for diagnosing and maintaining electrical systems. Digital and clamp-on multimeters measure voltage, current, resistance, and continuity with high accuracy, helping identify faults and verify system performance.

Ardent’s auto or manual ranging digital multimeters feature an Automatic terminal Blocking System (ABS), to secure proper lead connection, and their clamp-on multimeters have rotary clamp jaws that allow the user to align the clamp in the orientation of busbar/conductor while keeping the display and keys facing the user. A specialized insulation tester, also equipped with an ABS, provides quick, targeted checks to ensure equipment safety and functionality. Accessories such as test leads, clips, temperature adapters, and more enhance measurement precision, safety, and accessibility in tight spaces.



About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/

Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Image Download