Captron SENSORswitches are capacitive pushbuttons which are activated without pressure, using a hand or other parts of the body. The buttons have a determinate sensing distance, which may be altered by varying the approach speed and/or damping factor. A quickly approaching finger will achieve a higher sensing distance than a slowly approaching finger. A hand, with its larger damping surface, will achieve a greater sensing distance than a finger at the same speed.

These capacitive pushbutton switches are easily installed via M8 connections, use touch control with no mechanical pressure required and offer visual touch feedback through LED signals. The switches are IP69K rated and shock-resistant, vandal proof, 100% water/oil-proof.
These capacitive sensor switches are available in 22mm, 50mm and 60mm mounting diameters. Construction materials include plastic and stainless steel, aluminum or polycarbonate. Corresponding 22mm LED signal indicator lights are also IP69K rated and have a 20mm diameter illuminated area; green, red, yellow, white, orange, and magenta signal colors are available.
Available switch types are: static, the output signal is continuously on as long as the sensor area is activated; dynamic, the output signal length is limited to settable milliseconds when the sensor area is activated; and toggle, the output signal turns on when the sensor area is activated and stays on until the sensor area is activated again.
Capacitive pushbutton sensor switches from AutomationDirect start at $59.00 and have a 1-year warranty.
Learn more by visiting: www.automationdirect.com/capacitive-switches
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com