December 13, 2023 – AutomationDirect has added new Code barcode scanners to their portfolio of identification products. CR1500 series barcode scanners are compact hand-held devices with a dual-field optical platform that adds the ability to read laser etched, DPM, or high-density codes.
CR5000 series barcode scanners are table-top presentation mode scanners that facilitate hands-free operation. They have advanced data formatting that provides dependable data integration into any platform, system, or solution including iOS applications.
CR2700 series barcode scanners are high-end cordless scanners that use Bluetooth® 5 communications for secure, wireless data transmission, and glare reduction technology for reading barcodes on shiny surfaces.
An assortment of new accessories includes more communications cables and batteries/charging systems for the CR2700 series scanners.
The New Code barcode scanners start at $242.00. The Code CR1500 series barcode scanners come with a 5-year warranty; the CR5000 and CR2700 series have a 3-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo