September 17, 2025 – AutomationDirect has added Dold residual current monitors which detect leakage currents in grounded AC and DC systems, deliver early warning and alarm outputs with wide adjustment ranges, and support preventive maintenance and customized fault responses while minimizing unnecessary trips.
The RN5883 series AC/DC monitors work with external ND5015 residual (differential) current transformers to detect insulation faults, leakage currents, and broken conductors. When residual currents exceed user-defined thresholds, they provide early alerts to help prevent equipment damage, operator injury, and unplanned downtime. These current monitors feature selectable trip points (10mA to 3A), an analog output (0–10 VDC) proportional to the residual current, user-configurable warning and alarm outputs (SPDT relays) with adjustable time delays and manual reset, and an LED bar graph for real-time visual feedback of the measured current.
The ND5015 series AC/DC transformers combine Hall effect and CT technologies to measure residual currents in grounded systems. All monitored conductors, including neutral, pass through the sensor aperture, which outputs a differential signal to an RN5883 monitor for evaluation.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Image Download
Download: Web Friendly Image Download