Since 1977, Ever Motion Solutions has been a trusted leader in industrial automation, designing and manufacturing high-performance motion control solutions including stepper, brushless motors and drives.
The company uses its nearly 50 years of expertise to simplify motion control for customers worldwide and deliver reliable, durable products with an emphasis on innovation. Founded by engineer Felice Caldi, Ever Motion Solutions is family-owned, employing 85 people and producing over 110,000 drives every year.
Every drive and motor undergoes 100% testing, which demonstrates an unwavering attention to detail. The company believes that quality is the result of intelligent effort, building every product to meet the highest international standards. Ever Motion Solutions is certified for excellence with multiple certifications, including ISO 9001:2015 certification by TÜV SÜD, CE marking, UL certification for the U.S. and Canada and full compliance with RoHS and REACH regulations.
“For us, certifications aren’t just labels. They are embedded in the way we design, build and create our solutions,” says Felice Caldi, Founder and CEO.
Made In Italy
Headquartered in Lodi, Italy, with R&D and drives production facilities in-house, Ever Motion Solutions ensures every stage of manufacturing is optimized for top quality. A new motors production unit opening later in 2025 will further enhance the company’s “Made in Italy” manufacturing and create a connected production hub in the Lodi area
Felice Caldi says “We are evolving, adapting our processes and mindset to meet the challenges of the dynamic and constantly advancing automation environment.”
From concept to shipment, the Ever Motion Solutions team designs and creates custom solutions, aiming to meet every aspect of a customer’s needs. In an increasingly automated world, they hold a steadfast belief that people are still the driving force of everything.
“Behind every detail, there’s a human touch,” adds Felice Caldi.
Future-Forward
Ever Motion Solutions is always looking to the future, investing an average of 30% of annual profits into research and development. The company is aligning with the new Industry 5.0 model, where technology integrates seamlessly into daily operations and sustainability and resilience are key values. By advancing human-machine collaboration and adopting green, smart technologies, it is enhancing production quality while reducing environmental impact. Two state-of-the-art photovoltaic systems now supply 50% of the energy required for drive manufacturing, underscoring Ever Motion Solutions’ deep commitment to sustainability and energy efficiency.
Ever Motion Solutions Products at Automation Direct
The Titanio family of stepper drives from Ever Motion Solutions deliver industry-leading quality and control. These high-performance vector drives support both open-loop and optional closed-loop control and feature advanced technologies like ELSE (Error Less Servo Efficient) for smoother, quieter, and cooler motor operation. Titanio drives include stall detection in open-loop mode, using back EMF to monitor motor faults and report stalling without encoder feedback. The high quality of the stepper drives is backed up by an impressive 3-year warranty.
For advanced configuration of the stepper drives, the free Ever Studio software download offers expanded microstepping resolutions, jogging/indexing, and a built-in oscilloscope for tuning and debugging.
Automation Direct also features Ever Motion Solutions accessories including power supply cables, motor and encoder cables, programming cables, and spare/replacement connectors.