September 8, 2021 – AutomationDirect’s safety product offering now includes IDEM hazardous area safety devices. These safety devices provide similar functionality to their general-purpose counterparts but offer explosion-proof switching in hazardous locations.
All of these devices are manufactured with ATEX Exd IIC T6 certified explosion-proof contact blocks, which are encapsulated to contain explosions and prevent the ignition of hazardous materials.
New IDEM explosion-proof safety devices include tongue interlock safety switches, safety limit switches, and safety cable-pull switches. These devices are an excellent choice for use in the oil, chemical, pharmaceutical, and other hazardous industries.
AutomationDirect has also extended its existing line of general-purpose safety cable-pull switches. This new line extension allows for emergency cable lengths of up to 250 meters.
IDEM hazardous area safety devices start at $459.00, new extended length general-purpose cable-pull switches start at $169.00, and both have a 1-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo