AutomationDirect has added more intrinsically safe isolation barriers from STAHL. These modules ensure only a safe amount of energy resides in an electrical circuit, installed in a potentially explosive atmosphere, so that no sources of ignition are created.
More digital, analog, and temperature modules, new frequency transmitter isolators, and a Zener Barrier for thermocouple signals have been added.
Additional accessories include a configuration kit for the temperature and frequency modules and replacement fuse kits for the Zener Barrier.
The new STAHL intrinsically safe isolation barrier modules start at $189.00 and come with a one-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo