January 15, 2025 – AutomationDirect has added Penn-Union compression lugs to provide a secure method of terminating electrical cables, especially high-power or large-diameter cables, to electrical equipment. Unlike mechanical lugs, that are screwed/clamped in place, these connectors are crimped onto the cable using the appropriate crimping tool for a permanent installation. These connectors are rated for copper conductors, have a beveled entry for easy cable insertion, and have color-coded barrels marked with die index numbers, making inspections and certified installations much simpler. Penn-Union compression connectors are certified to be installed using commonly found tools and do so without loss of agency certification.
Also included are Penn-Union compression lug tools, which feature a small head designed for use in confined spaces. The unique telescopic handle design (TDM) provides increased leverage when needed, and the tools support 8 AWG up to 500 MCM wire/cable.
The new Penn-Union compression lugs offer quick and easy cable/wire installation and start at $1.50. The Penn-Union compression lug tools start at $361.25.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo