August 11, 2021- AutomationDirect has added PS-AMC motion controllers designed to work seamlessly with select Productivity PLCs to provide accurate, coordinated, plug-and-play motion control. These controllers are capable of up to 4 coordinated axes of motion per controller (PS-AMC4) with differential encoder feedback for each axis and a maximum switching frequency of 1MHz. Up to 24 general-purpose high-speed inputs and 12 general-purpose high-speed outputs are also included.
Available in 1, 2, 3, or 4 axes models, AMC controllers are auto-discovered in the Productivity Suite programming software, which has numerous built-in motion instructions allowing for easy configuration of standard motion profiles, including flying cut-offs and rotary tables.
The Productivity1000 remote I/O module provides a low-cost remote I/O solution for both the P1-550 and P2-550 controllers. Up to 4 P1-RX remote modules can be used with the P1-550, and up to 8 can be used with the P2-550. That adds an additional 512 I/O points to the P1000 system, which did not offer remote expansion before, and an additional 1024 for the P2000 at a much lower cost than the existing P2-RS expansion module. All P1-RX modules and connected I/O are auto-discovered in the Productivity Suite programming software with pre-assigned tags for each I/O point that can be used right away in the ladder code or modified as needed.
The new PS-AMC Motions Controllers start at $284, and the P1-RX Remote I/O Module is priced at $85.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo