Press ReleasesPress Releases

More SureFrame T-Slotted Rail Profiles from AutomationDirect

SureFrame T-Slotted Rail Profiles

November 16, 2022 – AutomationDirect has added additional profiles of SureFrame t-slotted rails. The new 30mm x 60mm and 60mm x 60mm profiles added to the 30 Series lineup allow for greater project flexibility. These new profiles offer the same durability as existing SureFrame rails and are compatible with slotted rails/hardware from most other manufacturers.

SureFrame t-slotted rails can be ordered cut to length and are guaranteed against manufacturer defects for one year from the date of purchase.

The new SureFrame T-slotted Rail Profiles start at $0.21/inch.

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/

Editorial Contact:               Tina Gable

Phone:                                 678-455-1845

Email:                                  tgable@automationdirect.com

Download:                          High Resolution Photo