December 11, 2024 – AutomationDirect has added Teknokol Eco series HMI enclosures and suspension arm systems which are designed to work together to provide customized, adjustable HMI panels using a selection of components and cut-to-length arm profiles. These suspension systems allow the HMI to be relocated as needed for better HMI visibility and operator comfort.
The medium-duty TK060 series suspension arm system is designed for lighter loads while the TK120 series offers the same design flexibility but is a heavy-duty option for heavier enclosures. Both models use custom-ordered arm profiles that can be ordered precut to fit specific applications.
Several accessories have also been added, including various handle options that can be mounted on the sides or bottom of the enclosure and removable front plates.
Teknokol HMI enclosures start at $349.00, suspension arm system components start at $27.00, and accessories start at $26.00.
Learn more by visiting:
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo