June 28, 2023 – AutomationDirect is pleased to announce the launch of several IEC and compact limit switches under the new house brand, AchieVe. These new AchieVe limit switches are available in a selection of sizes and styles, including: These limit switches offer a variety of actuator styles, including plunger, lever, and a new pull-action…
June 28, 2023 – AutomationDirect has added E-T-A REX modular electronic circuit protectors to their selection of circuit protection devices. These protectors safeguard electrical circuits from overcurrent, short circuits, and other faults. Featuring a modular design, individual protection modules can be combined to meet specific circuit protection requirements, allowing for flexible configurations and easy installation….
Vacuum Gripper Advantages Modular gripper system kits provide a versatile way for designers and OEMs to quickly create material handling and robot end-of-arm tooling solutions.OEMs and designers put a lot of work into gripping systems because dropping a payload can lead to waste and downtime. Custom-engineered systems are often the norm, but these can be…
Once again, AutomationDirect PLC and other products have been highly ranked as voted on by automation professionals. AutomationDirect PLCs, HMIs, and motion controllers were recently recognized in the Control Design 2023 Readers’ Choice Awards for several categories. You can find the magazine issue online here. Each year, Control Design invites readers who identify themselves as…
June 14, 2023 – AutomationDirect has added quality tool bags and cases from C.H. Ellis to make transporting tools to/from a remote job location easier. Included in this addition is a mechanic’s tool bag made of black ballistic nylon with two carry handles, four interior and three exterior pockets on each side, and 2-snap flaps…
June 14, 2023 – AutomationDirect has added new multi-bit drivers from Megapro. These bit drivers are versatile screwdrivers designed to house a set of common or specialized screwdriver bits for a variety of industrial applications. Megapro bit drivers are available with various double-ended industrial grade S2 steel bits and have an alloy shaft that also…
June 14, 2023 – AutomationDirect has added the next generation CPU for the Productivity2000 PLC line. The P2-622 CPU has all the functionality of the original CPU including up to 50MB ladder memory, embedded OLED status display, remote I/O and multipurpose Ethernet 10/100Base-T (RJ45) ports, and a microSD card slot. In addition, this new CPU…
June 14, 2023 – AutomationDirect has added the 10 (1 inch), 15 (1.5 inches), and 40 (40mm) series of SureFrame rails, in standard and light weights. These new rails are offered with a UV-resistant black anodized finish, which provides a new aesthetic option in addition to the standard clear anodized finish that is available for…
June 7th, 2023 – AutomationDirect has added Spartan Scientific water valves to their offering of low-cost potable water components. These solenoid valves are suitable for use with potable water as well as a variety of other liquids, oils, and inert gases. Spartan water valves feature a 2-port (2-way), 2-position design with a normally closed configuration…
June 7th, 2023 – AutomationDirect has added Bryant pin and sleeve mechanical interlocks to their growing lineup of motor disconnects and controllers. These interlocks use pin and sleeve technology to conveniently connect and disconnect mobile equipment safely. By using matching Bryant pin and sleeve connectors with keyways, these interlocks safeguard against connecting devices of different…