Newsletter Volume 24 Issue 4
NewsletterNewsletter

Newsletter Volume 24 Issue 4

Product advice on easy, affordable modern control, IIoT implementationPlant engineers, electrical technicians, machine builders are among the users who need industrial-grade automation platforms so they can create practical control systems and advanced Industrial Internet of Things (IIoT) applications. Many of these projects are smaller-scale, perhaps 100 or fewer input/output (I/O) points, and these users require…
Saginaw Enviro-Therm® Series Enclosure Air Conditioners from AutomationDirect
Issue 48 -2022NewsNotebook IssuePress ReleasesPress Releases

Saginaw Enviro-Therm® Series Enclosure Air Conditioners from AutomationDirect

April 27, 2022 – AutomationDirect has added a new line of Saginaw enclosure air conditioners designed to efficiently keep the internal temperature of an electrical enclosure at a safe level, protecting the enclosed equipment from overheating and moisture damage. These air conditioners utilize closed-loop cooling to keep contaminants in the ambient air out of the…
The CLICK PLUS PLC is Voted as the 2021 Plant Engineering Magazine Product of the Year Bronze Award in the Control Systems category
Company TopicsIssue 48 -2022News

The CLICK PLUS PLC is Voted as the 2021 Plant Engineering Magazine Product of the Year Bronze Award in the Control Systems category

AutomationDirect’s CLICK PLUS PLC is the next generation platform for delivering reliable and familiar functionality for basic control applications, combined with advanced features like Wi-Fi, data logging, and increased security measures. All starting at just $89! On April 25, 2022 the AutomationDirect CLICK PLUS PLC was announced as the Plant Engineering 2021 Product of the…
Acme Electric Encapsulated Core General Purpose Transformers and Buck-Boost Transformers from AutomationDirect
NewsPress ReleasesPress Releases

Acme Electric Encapsulated Core General Purpose Transformers and Buck-Boost Transformers from AutomationDirect

March 30, 2022 – AutomationDirect has added new 1-phase encapsulated core general purpose transformers and buck-boost transformers from Acme Electric. These general-purpose transformers use electrical grade silica and resin compounds to completely enclose the core and coil to prevent corrosion and insulation deterioration. They are available in various voltages and sizes from 0.25 to 25…
Newsletter Volume 24 Issue 3
NewsletterNewsletter

Newsletter Volume 24 Issue 3

Cybersecurity Best PracticesContemporary industrial cybersecurity measures require the right hardware and software technologies, but must also incorporate user best practices.Now that most intelligent automation devices include wired or wireless network connectivity, end users can easily obtain valuable equipment data. However, the more capable PLCs, HMIs, and other devices making this possible also mean that designers need…
New Gladiator GCB Series Molded Case Circuit Breakers from AutomationDirect
NewsPress ReleasesPress Releases

New Gladiator GCB Series Molded Case Circuit Breakers from AutomationDirect

March 23, 2022 – AutomationDirect has added Gladiator GCB series molded case circuit breakers to their lineup of circuit protection devices. Gladiator MCCBs are designed to reliably protect circuits and equipment from thermal overloads, short circuits, and ground faults. Available in two or three-pole configurations, these high-performance circuit breakers are offered in seven frame sizes…