February 2, 2020 – Intended for the user who doesn’t require a built-in HMI display, needs a larger display, or would rather strictly use the C-more mobile app, the C-more® EA9 series remote (headless) HMI unit provides all the functionality of an EA9 touch panel without the extra cost of a touchscreen interface. The headless…
DataMax Extreme® Industrial Profinet cables are a two-pair shielded construction with 22AWG twisted pair conductors and 7/30 stranded tinned copper with color coded high-density polyethylene insulation. Shielded constructions include both a tinned copper braid shield and aluminized polyester foil overall shield. The cable’s outer jacket is pressure extruded Thermoplastic Elastomer (TPE) with excellent moisture, chemical,…
New Industrial Grade Open-Source CPU The open-source Productivity®Open platform provides all the great features of a standard Arduino plus the added power and reliability of an industrial controller. The processor circuit of the P1AM-100 Arduino-compatible CPU is designed to mimic the Arduino MKRZero microcontroller. The P1AM-100 is compatible with most available Arduino MKR format shields, and/or…
AutomationDirect’s STRIDE communication products provide reliable connectivity to industrial controllers and field devices. The STRIDE Field I/O family of modules provides a simple and economical means to connect inputs and outputs to a Modbus TCP communications network via Ethernet 10/100 Base-T. Each module operates as a standalone Modbus TCP server, and can be remotely configured…
The open-source Productivity®Open platform provides all the great features of a standard Arduino plus the added power and reliability of an industrial controller. The processor circuit of the P1AM-100 CPU is designed to mimic the Arduino MKRZero microcontroller. The P1AM-100 is compatible with most available Arduino MKR format shields, and/or the industrially-hardened ProductivityOpen shields, and…
Wenglor rectangular 50 x 50 x 20mm photoelectric sensors from AutomationDirect include diffuse with background suppression, retroreflective, retroreflective for transparent objects, and through-beam models. The popular size of these Wenglor sensors makes them ideal as drop-in replacements for other higher-cost rectangular photoelectric sensor brands. Sensing ranges vary from 1200mm for background suppression sensors to 20m…
Hammond Manufacturing® enclosures, including disconnect, stainless, commercial, console and other enclosure styles, are now available from AutomationDirect along with our existing AttaBox®, Hubbell-Wiegmann® and Integra enclosure offerings. A wide variety of metal and non-metal enclosures, rated NEMA 1, 3, 3R, 3S, 4, 4X, 6, 6P, 12 or 13, are available in wall-mount, floor-mount and freestanding…
A key AutomationDirect value is to be a responsible, involved citizen of the communities where team members live and work. That’s one of the reasons the company has served for the past two years as an employer for Internship Forsyth which gives students the opportunity to learn real-world skills by working at local companies. The…
For the ninth year in a row, Automation World readers have voted for their “First Team” suppliers in PMMI Media Group’s 2020 Leadership in Automation program. This year, AutomationDirect made “First Team” in the following categories: HMI Hardware HMI Software PLCs/PACs First Team Honoree Automation World, a leading business magazine serving automation professionals, asks their…
AutomationDirect ProSense® digital panel meters in 1/32 and 1/8 DIN sizes are AC or DC powered and feature IP65-rated meter faces, simple menu-driven pushbutton configuration, and accept a wide variety of input signals. Available outputs include alarm relays, milliamp current, and sensor excitation voltage options. New process-display options now include (depending on series) AC or…