AutomationDirect’s ProSense DPG1 digital pressure gauges are ideal for industrial and general purpose applications requiring an accurate and reliable device with easy to read digital display.
Recently, AutomationDirect’s very own Rick Folea, Senior Technical Marketer, was featured on North Fulton Business Radio speaking about STEM and how local Robotics programs are helping kids learn and become excited about science, technology, engineering, and math. The complete interview can be heard here. A Little Background Since 2006, AutomationDirect has been sponsoring Robotics programs…
With the launch of the newest Do-more! controller, the BRX PLC, AutomationDirect released an enhanced version of the Do-more! Designer programming software. Do-more! Designer 2.0 has many new features added to improve programming efficiency.
AutomationDirect has added a new line of high precision limit/position switches from Metrol. Traditional limit switches and even electronic proximity sensors are limited in terms of accuracy and repeatability. These cost-effective, ultra-precise mechanical limit switches have repeatability down to 10, 5, 3, and even 0.5 microns (µm) depending on the specific model.
New IronHorse Shaft Mount Gearboxes (speed reducers) from AutomationDirect feature shafts and gears manufactured from the highest grade steel, case hardened and precision ground to AGMA standards for long lasting durability.
AutomationDirect has added two new feature-enhanced CPUs to its DirectLOGIC DL405 programmable logic controller product line. The D4-454 and D4-454DC-1 provide all the capabilities of the D4-430, D4-440 and D4-450 CPUs, using updated microprocessor technology allowing the D4-454 to be the CPU of choice for the DL405 family.
Two new C-more Micro HMI touch panels are now available from AutomationDirect. C-more Micro panels display text, graphics, and bitmaps to effectively communicate critical HMI data to the operator.
New design improvements have been made to AutomationDirect’s ProSense® line of temperature switches. TSDA25 series temperature switches are a direct replacement for the TSD25 series and provide higher accuracy and a standard sized 6mm diameter probe.
AutomationDirect has expanded its sensors offering to include wide area sensors for object detection. The new area sensors from Micro Detectors (MD) are multi-beam, through-beam sensors with emitter and receiver elements used for detecting the presence of any object by sensing the light beam intensity returning from the receiver. The area sensors have an IEC…
Hope everyone had a great relaxing long weekend! We thank those who courageously gave their lives and those who continue to fight for the freedoms we have today. In this month’s issue there is an application story on how an AutomationDirect Do-more H2 Series Programmable Logic Controller CPU was used to upgrade an outdated gas…