June 14, 2023 – AutomationDirect has added new multi-bit drivers from Megapro. These bit drivers are versatile screwdrivers designed to house a set of common or specialized screwdriver bits for a variety of industrial applications. Megapro bit drivers are available with various double-ended industrial grade S2 steel bits and have an alloy shaft that also…
June 14, 2023 – AutomationDirect has added the next generation CPU for the Productivity2000 PLC line. The P2-622 CPU has all the functionality of the original CPU including up to 50MB ladder memory, embedded OLED status display, remote I/O and multipurpose Ethernet 10/100Base-T (RJ45) ports, and a microSD card slot. In addition, this new CPU…
June 14, 2023 – AutomationDirect has added the 10 (1 inch), 15 (1.5 inches), and 40 (40mm) series of SureFrame rails, in standard and light weights. These new rails are offered with a UV-resistant black anodized finish, which provides a new aesthetic option in addition to the standard clear anodized finish that is available for…
June 7th, 2023 – AutomationDirect has added Spartan Scientific water valves to their offering of low-cost potable water components. These solenoid valves are suitable for use with potable water as well as a variety of other liquids, oils, and inert gases. Spartan water valves feature a 2-port (2-way), 2-position design with a normally closed configuration…
June 7th, 2023 – AutomationDirect has added Bryant pin and sleeve mechanical interlocks to their growing lineup of motor disconnects and controllers. These interlocks use pin and sleeve technology to conveniently connect and disconnect mobile equipment safely. By using matching Bryant pin and sleeve connectors with keyways, these interlocks safeguard against connecting devices of different…
May 31, 2023 – AutomationDirect has added new WERMA eSIGN series LED signal towers to their lineup of pre-assembled stacklights. These new signal towers, available in 9- and 15-tier models, feature a variety of customizable operating modes and lighting effects. eSIGN signal towers provide full-surface signaling with electronic modularity and can operate as a traditional…
AutomationDirect has added new IronHorse manual motor protectors, contactors, thermal overload relays, and a wide variety of supported accessories to their growing lineup of motor control products. The IronHorse HMC series contactors are a very economical solution and feature an advanced design with a sealed structure to prevent arc flash exposure; electronic coils are available…
May 24, 2023 – AutomationDirect has added the next generation of the popular C-more HMI product line. The CM5 HMI series offers lower cost, high-performance HMIs in sizes from 4 inches to an impressive 22 inches. These HMIs have an amazing 1.6 GHz processor in the larger units (10” and above), 43 Mbytes of memory,…
May 10th, 2023 – AutomationDirect has released several new modules for the Productivity family of controllers. Two new lower-cost, high-resolution, four-channel analog input modules, supporting current (0-20 mA) or voltage (0-10 VDC) signals, are now available for the Productivity1000 PLC. The ProductivityOpen Arduino-based controller line now offers a 2-port serial communications shield that provides a…
May 10th, 2023 – AutomationDirect’s newest addition of A-coded sensor and signal connection cables from Murrelektronik provides easy and reliable connections between panels and field devices. These cables offer several configurations including axial or right-angle female M8 or M12 screw-lock connector to pigtail, axial male to axial female with M8 or M12 screw-lock connectors, and…