What is Productivity2000?
+Tech TopicsAutomation NotebookIssue 33 - 2015Learning ResourcesNotebook IssueProductProgrammable ControlTechnology Brief

What is Productivity2000?

It’s not just the low price, but the incredible built-in features that make our Productivity2000 a must-have controller. As the newest programmable logic controller from AutomationDirect, the Productivity2000 (P2000), is built around a compact modular form factor that allows both fit and functionality in a small space. But, what is Productivity2000? In this introduction we…
Ease of Motion with Do-more PLC and the H2-CTRIO2
+Tech TopicsAutomation NotebookIssue 24 - 2012Learning ResourcesNotebook IssueProductProgrammable ControlTechnology Brief

Ease of Motion with Do-more PLC and the H2-CTRIO2

Part of the vision for the Do-more PLC control engine was to make maximum use of Host Engineering’s next generation High Speed Counter and Pulse Output module, the H2-CTRIO2. Pairing this new module with a Do-more CPU creates a solid motion control package that is easier to use than its predecessors while offering more flexible…
HMIs and PC Control: Upwardly Mobile With Upscale Connections
+Tech TopicsAutomation NotebookCommunicationsIssue 1 – 2004Learning ResourcesNotebook IssueProductProgrammable ControlTechnology Brief

HMIs and PC Control: Upwardly Mobile With Upscale Connections

Remember when you had to be an artist to design HMI faceplates that resembled your process? Remember configuring your HMI software by filling in cryptic addresses and values, something resembling the Microsoft® Windows™ registry? Remember when your HMI was a dedicated system that only connected to a single process? Or when it was cool to…