Recent Posts

+Tech TopicsHand Tools &Test EquipmentIssue 55, 2025Learning ResourcesNotebook IssueProductTech Thread

Outfitting Your Panel Shop to be Safe and Efficient

AutomationDirect has created an extensive portfolio of professional-grade control panel products, tools, and test equipment, all readily available at reasonable cost so that shops can equip their technicians to deliver high-quality results. By Zach Ganster, AutomationDirect The “good/better/best” concept is familiar to most people. When it comes to obtaining anything we use in our daily…
AutomationDirect SpotlightIssue 55, 2025Notebook IssueStudent SpotlightStudent Spotlight

Diving Deep into STEM Education

This student team gained valuable STEM experience by developing an underwater remote operated vehicle, and they accelerated their efforts by using commercially available industrial-grade components. By: Geoff Gardener, North Paulding High School Exploration of both the deep sea and of outer space share a lot in common. Both are extremely unforgiving environments where it is…
+Tech TopicsIssue 55, 2025Learning ResourcesNotebook IssueProductSafetyTech Thread

Beyond Safety Slogans: Cultivating a Workforce Culture to Protect People and Productivity

By Travis Morris, Safety Administrator, AutomationDirect As we recognize National Safety Month this June 2025, it’s the perfect time to reflect on how industrial safety has evolved alongside technological advancement. At AutomationDirect, we’ve seen firsthand how the safety landscape in manufacturing and logistics continues to advance rapidly, creating both new challenges and unprecedented opportunities for…
Issue 55, 2025Notebook IssueProductSafety

Building a Safety Component Fortress Around Equipment

By: Larry Reynolds, AutomationDirect Safety systems play a crucial role in industrial equipment, protecting personnel, guarding against machine damage, and minimizing unscheduled downtime. To make a machine totally safe, we could build a wall around it, cut the power, send staff home, and lock the doors after them. That approach isn’t particularly practical, however. Instead,…
Uncategorized

Issue 55, 2025

In the world of manufacturing, efficiency and productivity often take center stage. However, there’s one element that must always be prioritized above allelse: employee safety. Recognizing that June is National Safety Month, AutomationDirect is dedicating much of this issue of NOTEBOOK to addressing the issuesthat impact safety in the manufacturing workplace — from culture to…
Issue 55, 2025Notebook IssueUncategorized

Brainteasers, Issue 55, 2025

Polka Dot Remainder Find the area of the blue shaded portion in each figure below: Area Sensors Speaking of Area – did you know that AutomationDirect offers multiple types of Area Sensors? Also known as Measuring Light Grids, these sensors can detect the presence of an object within the grid, AND measure that object’s height….
NewsPress ReleasesPress Releases

Helukabel HELUKAT Ethernet and Profinet Cable from AutomationDirect

April 30, 2025 – AutomationDirect has added Helukabel’s HELUKAT industrial Ethernet and Profinet cables featuring a halogen-free, flame-retardant, and durable construction built to support a variety of industrial requirements. New Type B, Type B Hybrid (with power conductors), Type R, and Type C Profinet cables are designed to provide reliable data transmission in dynamic or…
NewsPress ReleasesPress Releases

Lika® Draw Wire Encoders from AutomationDirect

April 30, 2025 – AutomationDirect has added Lika draw wire linear measurement devices, also known as string encoders or string potentiometers, which use a steel cable wrapped on a spring-loaded reel to measure distance. The reel is connected to a rotary encoder or potentiometer that can provide very accurate feedback on how far the steel…
NewsletterNewsletter

Newsletter Volume 27 Issue 4

How to Choose a Sensor for the Production Environment Sensors play essential roles in the modern production environment, capturing data on position, speed, proximity, pressure, temperature, level, flow, current, voltage, and more. There is such a wide variety of sensors on the market that finding the right device for your application can seem overwhelming. It…
NewsPress ReleasesPress Releases

GC Valves NSF Lead-Free Brass Water Valves from AutomationDirect

April 23, 2025 – AutomationDirect has added GC Valves 71 series 2-port water valves, which are constructed of durable lead-free brass. They are certified to NSF/ANSI 61 and have NSF-approved EPDM diaphragms. They are a great choice for drinking water applications and are ported for the most popular NPT sizes (up to 2”) with a…
Content CollectionsProductProgrammable Control

Get Ahead with Node-RED

Node-RED is a visual programming tool for connecting physical hardware devices, APIs, and online services together as part of the Internet of Things. It was originally developed by the IBM Emerging Technology Services team and is now a part of the OpenJS Foundation. Node-RED’s low-code, drag-and-drop interface makes it easy to create complex data flows…
NewsPress ReleasesPress Releases

ICON Process Controls Truflo® TKM Series Paddle Wheel Liquid Flow Meters from AutomationDirect

April 9, 2025 – AutomationDirect has added ICON Process Controls Truflo® TKM series paddle wheel liquid flow meters that provide reliable, full-pipe liquid flow measurement with exceptional long-term performance. These rugged, highly repeatable sensors deliver outstanding value with no scheduled maintenance required. Built with a chemically resistant PVC body, they are ideal for corrosive liquid…
AutomationDirect SpotlightSupplier ProfilesSupplier Profiles

Supplier Profile: Lika

Lika Electronic specializes in encoders and position measuring systems, including incremental and absolute, optical and magnetic, rotary and linear encoders, incremental & absolute magnetic measurement systems, rotary actuators, displays, signal converters and encoder interfaces. Starting in 1982 as a family-owned business, Lika Electronic has grown to become a forward thinking innovative, global company. Over the…
Uncategorized

AutomationDirect’s C-more CM5 Headless HMI Nominated for Control Engineering 2025 Product of the Year Awards

The C-more CM5-RHMI headless HMI offers all the features of the traditional touchscreen C-more line, but in a compact and connectable low-cost form factor. AutomationDirect’s C-more CM5-RHMI has been nominated for Control Engineering’s Product of the Year program in the human-machine interface (HMI) category. Help us bring home the gold by visiting https://survey.alchemer.com/s3/8206433/f8132b621423 and casting…
Process Sensing & ControlProduct

Solving Frequency Signal Conditioner Challenges

Complex high-frequency signaling challenges, for both existing and new applications, can be solved using signal conditioners. Frequency signal conditioners—designed to handle high-frequency pulse signals from sensors and convert them into other useful automation signals—are an important industrial automation design component for both new and retrofit applications. High-frequency pulses may be generated from a proximity sensor…
NewsletterNewsletter

Newsletter Volume 27 Issue 3

Six Tips to Help You Build a Better, Safer Machine Safety is an essential aspect of machine design and operation, protecting personnel, guarding against equipment damage, and maximizing productivity. The purpose of a safety system is to bring a machine to a known safe state as quickly as possible after a safety sensor detects a…
NewsPress ReleasesPress Releases

Datasensing SH4 Category 4/Type 4 Safety Light Curtains from AutomationDirect

March 26, 2025 – AutomationDirect has added Datasensing SH4 series 14mm finger and 30mm hand safety light curtains that are available in basic models with automatic restart or standard models, which include external device monitoring (EDM) and an optional manual restart. Body protection models in 300 or 400mm resolution are available only in the standard…
NewsPress ReleasesPress Releases

Wenglor OPT25 Series Laser Distance Measurement Sensors from AutomationDirect

March 26, 2025 – AutomationDirect has added Wenglor OPT25 series laser measurement sensors that offer best-in-class distance sensing for ranges within 1 meter. These sensors are IO-Link v1.1 compatible, employ a Class 1 red or Class 2 blue laser, use triangulation to measure distances with extreme accuracy, and can reliably detect tiny objects with a…
NewsPress ReleasesPress Releases

Autonics Miniature Photoelectric Sensors from AutomationDirect

March 26, 2025 – AutomationDirect has added Autonics BTF, BTS, and BPS series miniature photoelectric sensors featuring ultra-compact slim or narrow housings that are easy to install in tight spaces. The lineup includes:        These miniature sensors offer sensing distances up to 3m, durable PBT thermoplastic housings, and an IP67 protection rating. They…
NewsPress ReleasesPress Releases

ProSense Linear Potentiometers from AutomationDirect

March 19, 2025 – AutomationDirect has added ProSense linear potentiometers that offer reliable and consistent position measurement while delivering exceptional value and performance. These position sensors measure linear displacement by converting mechanical movement into a resistive output. Typically, they require a signal conditioner or a 10 VDC supply to provide an analog signal for a…
NewsPress ReleasesPress Releases

IronHorse® Aluminum Worm Gearboxes with IEC Input from AutomationDirect

March 19, 2025 – AutomationDirect has added IronHorse worm gearboxes with IEC inputs that offer all the same features and advantages as our existing aluminum models, including 30mm to 75mm frame sizes, 10:1 to 100:1 ratios in most sizes, and maintenance free operation.  They are factory filled with synthetic oil and their double lip oil…
NewsPress ReleasesPress Releases

METEcon Multi-Wire Connectors from AutomationDirect

March 12, 2025 – AutomationDirect has added METEcon multi-wire connectors that feature quality and cost-effective inserts and housings. Inserts are available in multiple pole configurations from 2 poles plus ground up to 108 poles plus ground, with screw or crimp termination types and sizes ranging from 26 to 12 AWG, 10 to 80 Amps. METEcon…
AutomationDirect SpotlightSupplier ProfilesSupplier Profiles

Supplier Profile: Master Appliance

Headquartered in Racine, WI, Master Appliance has been a leader in heat tool innovation since the 1950s. The company introduced the first portable industrial heat gun to North America, coining the term “heat gun” and revolutionizing how industries apply heat for tasks such as heat shrink packaging, drying parts, shrinking plastics, paint stripping and shaping…
Issue 55, 2025NewsNotebook IssuePress ReleasesPress Releases

New Option Slot and Stackable I/O Modules for the CLICK PLC Family from AutomationDirect

February 26, 2025 – AutomationDirect has added new specialty modules for the CLICK PLC family. CLICK PLUS CPUs offer the utmost versatility with up to two option slots for custom I/O configurations. These option slots also allow for specialty modules, including the C2-DCM serial communication module and the new C2-NRED and C2-OPCUA modules. The C2-NRED…
Issue 55, 2025NewsNotebook IssuePress ReleasesPress Releases

Ever Motion Solutions Titanio Series Stepper Drives from AutomationDirect

February 26, 2025 – AutomationDirect has added the new Titanio series of stepper drives from Ever Motion Solutions®. These drives offer peak performance, a rich feature set, and work seamlessly with AutomationDirect SureStep® stepper motors.  Three new drives are available with two open-loop (no encoder feedback) models and one open/closed-loop version (a motor-mounted encoder provides…
Uncategorized

Issue 54, 2025

Easy, Educational, and Entertaining Automation At AutomationDirect, the goal is to educate customers on the best industrial products for their applications. The mission is also about making industrial control easy — and sometimes even entertaining. In this issue of NOTEBOOK, we demonstrate how AutomationDirect delivers on these important objectives. Here, we focus on modern PLC…
Issue 54 - 2025Notebook IssueProcess Sensing & ControlProduct

How to Choose a Sensor for the Production Environment 

By: Andrew Waugh Sensors play essential roles in the modern production environment, capturing data on position, speed, proximity, pressure, temperature, level, flow, current, voltage, and more. There is such a wide variety of sensors on the market that finding the right device for your application can seem overwhelming. It doesn’t have to be. The goal…
Issue 54 - 2025Notebook IssueProductProgrammable Control

How Low-Code and No-Code Visual Programming Tools Can Simplify and Accelerate Seamless Industrial IoT Connectivity

In this article, we explore the transformative impact of low-code/no-code PLC programming in industrial automation with Tim Shippy, a veteran AutomationDirect Product Engineer. With a wealth of experience spanning decades in industrial and enterprise software development, Tim has been at the forefront of integrating industrial systems with enterprise connectivity. His expertise in both traditional and…
Issue 54 - 2025Notebook IssueProductSafety

Six Tips to Help You Build a Better, Safer Machine

By: Joshua Draa and Larry Reynolds, Automation Direct Safety is an essential aspect of machine design and operation, protecting personnel, guarding against equipment damage, and maximizing productivity. The purpose of a safety system is to bring a machine to a known safe state as quickly as possible after a safety sensor detects a hazardous condition…
AutomationDirect SpotlightIssue 54 - 2025Notebook IssueStudent SpotlightStudent Spotlight

Cultivating Curiosity with Automated Edu-tainment

Crafting agricultural education experiences that are also fun is a specialty requiring a mix of creativity and technology. Byline: Justin Hiemstra, Heemer Crafted Capturing the interest of a young person today can be a tough task, especially considering the proliferation of mobile devices and the obsession with screen time. However, there are still important opportunities…
Application StoriesFood and BeverageHMIIndustryIssue 54 - 2025Operator InterfaceProduct

Recipe for Success: Automation Proves to Be a Key Ingredient

The right mix of automation elements is crucial for creating a consistent process yielding high-quality donuts and baked goods. By Roger Dyer, Mel-O-Cream Donuts International Mel-O-Cream, a commercial bakery in Springfield, IL, has been baking and perfecting donuts since 1932. From measuring precise ingredient amounts and maintaining a consistent mixing process, to ensuring uniform dough…
NewsletterNewsletter

Newsletter Volume 27 Issue 2

Unshackling Industrial Data Access Modern consumers are increasingly familiar with tailored experiences, abundant information, and generally getting things “their way.” Those working in the industrial manufacturing and automation sectors, on the other hand, have not always enjoyed such flexibility. Fortunately, hardware and software advancements mean that access to valuable industrial sourced data is easier, more…
Issue 54 - 2025Notebook Issue

BrainTeasers - Issue 54, 2025

Application Complication The programmer for the gasket applicator robot at the puzzle factory noticed that there were a number of different tool paths that could be used to program the gasket path required for a new mechanical puzzle.  The complete pattern is shown below.  He must apply the gasket in a continuous bead along all…
AutomationDirect SpotlightSupplier ProfilesSupplier Profiles

Supplier Profile: CITO Products, Inc.

At the London International Exhibition in 1862, Alexander Parkes introduced the world’s first man-made plastic. His creation launched the beginning of the plastics industry, which would grow exponentially during the next 100 years to serve both manufacturers and consumers in many ways. In 1965, Horst Wieder founded CITO Products, Inc. as a toolmaking, machining, and…
NewsletterNewsletter

Newsletter Volume 27 Issue 1

Build Better Machines Faster Using Today’s Enhanced Motion Controllers and PLCs High-performance servo motion is now more affordable and accessible than ever due to integrated controllers, making the technology viable even for applications which could not formerly support the cost or complexity of traditional implementations. Learn more The Master Controller of Motors Everyone knows that…
Issue 55, 2025NewsNotebook IssuePress ReleasesPress Releases

BLOCK Open Core Control Transformers from AutomationDirect

February 12, 2025 – AutomationDirect has added BLOCK CT and USTE series open core control transformers to provide a flexible solution for stepping down a wide range of voltages from 208 to 600 VAC. The BLOCK CT series is made in the USA and offers a rugged design specifically engineered for isolation, lighting, or signaling…
NewsPress ReleasesPress Releases

Additional Murrplastik Cable / Hose Drag Energy Chains and Accessories from AutomationDirect

February 12, 2025 – AutomationDirect has added Murrplastik MP10 series cable/hose drag chains and chain brackets to their growing selection of wire and cable management products. Drag chains route cables/hoses to moving components and help to extend cable/hose life, provide protection for personnel, and reduce equipment downtime and repair costs. The MP10 series is built…
AutomationDirect SpotlightStudent SpotlightStudent Spotlight

FIRST Robotics Competition 2025 Digital Animation Award Winners

This award, sponsored by AutomationDirect, celebrates the art of digital animation and its close relationship to STEAM (Science, Technology, Engineering, Art, and Mathematics). The 2025 Digital Animation Award is offered to help encourage students to cultivate skills in design and creation of animation including, but not limited to, storytelling, creativity, use of computer software, and…
NewsPress ReleasesPress Releases

WAGO Lever Nuts from AutomationDirect

February 5, 2025 – AutomationDirect has added WAGO splicing connectors to their selection of wiring solutions. The 221 series LEVER-NUTS® are equipped with WAGO’s CAGE CLAMP® spring technology, allowing quick and easy connection of all conductor types of different cross sections using two-, three-, and five-wire connectors without soldering or using tools. The 221 series…
Issue 55, 2025NewsNotebook IssuePress ReleasesPress Releases

WEG CFW320 AC VFDs and SSW900 Soft Starters from AutomationDirect

February 5, 2025 – AutomationDirect has added general-purpose WEG CFW320 AC drives and full-featured SSW900 soft starters. The CFW320 series VFDs offer all the features of the existing CFW300, including a compact size, a built-in operator interface (HMI), and an embedded SoftPLC, but provide support for 460 VAC and Ethernet communications. These drives support 230 VAC 3-phase…
NewsPress ReleasesPress Releases

Additional Murrplastik Cable Entry Frames and Grommets from AutomationDirect

February 5, 2025 – AutomationDirect has added more Murrplastik frames and grommets to their current offering of cable entry systems. Cable entry frames used in conjunction with the required grommets provide easy cable installation through an enclosure and strain relief while maintaining environmental ratings. This expansion adds more frame sizes to our existing KDL/D and…
Issue 55, 2025NewsNotebook IssuePress ReleasesPress Releases

Gladiator GPB1 and GPB2 Enclosed Style Terminal Blocks from AutomationDirect

January 29, 2025 – AutomationDirect has added Gladiator GPB1 and GPB2 series enclosed-style terminal blocks to provide a safe and reliable way to connect multiple electrical circuits to a single power source. The GPB1 series terminal blocks are ultra-compact, offering time-saving multiple wire connection options for a variety of control panel applications. Push-in spring connections…
NewsPress ReleasesPress Releases

More Stahl Intrinsically Safe Zener Barriers from AutomationDirect

January 29, 2025 – AutomationDirect has added additional Zener barriers from STAHL to isolate various control signal types from hazardous environments. For automated systems installed in potentially explosive atmospheres (ex., oil and gas production), extra precautions must be taken to ensure the electrical circuits do not become ignition sources. Properly grounded Zener barriers isolate the…
Issue 55, 2025NewsNotebook IssuePress ReleasesPress Releases

Schmersal Configurable Safety Relays from AutomationDirect

January 22, 2025 – AutomationDirect has added configurable and programmable safety relays from Schmersal. Many safety systems require more than one specialty safety relay but do not justify the need for a safety controller. Schmersal PROTECT SRB-E configurable relays are easy to set up and reduce the number of safety relays required for a machine…
Issue 55, 2025NewsNotebook IssuePress ReleasesPress Releases

Dold VARIMETER Series Voltage and Phase Monitoring Relays from AutomationDirect

January 22, 2025 – AutomationDirect has added Dold VARIMETER series voltage and phase monitoring relays to safeguard electrical equipment and prevent costly downtime by evaluating voltage levels and phase sequences. These relays provide early detection and response to abnormalities such as undervoltage, overvoltage, phase loss, phase reversal, and phase imbalance. The VARIMETER series monitoring relays…
NewsPress ReleasesPress Releases

PBC Linear Guide Tracks with Slides and Roller Pillow Block Bearings from AutomationDirect

January 22, 2025 – AutomationDirect has added seven new sizes of PBC linear guide tracks with slides in lengths up to 2000mm.  The guide tracks are ceramic-coated 6061-T6 aluminum, paired with a self-lubricating slide. The slides have a proprietary PTFE (FrelonGOLD®) plain bearing bonded to the mating surface. These guide tracks and slides are rated…
Issue 54 - 2025Notebook IssueOperator InterfaceProductProgrammable Control

Unshackling Industrial Data Access

Modern PLCs and HMIs make it easy to implement extensive data connectivity and analytics. By: Damon Purvis, AutomationDirect Modern consumers are increasingly familiar with tailored experiences, abundant information, and generally getting things “their way.” Those working in the industrial manufacturing and automation sectors, on the other hand, have not always enjoyed such flexibility. Fortunately, hardware…
NewsPress ReleasesPress Releases

ProSense FLG Series Detection Light Grids from AutomationDirect

January 15, 2024 – AutomationDirect has added ProSense FLG series detecting light grids that offer a cost-effective solution for object detection and feature a simple setup with no programming required. They have no dead zone on the full detection height and are perfect for a variety of applications, such as material handling, counting, and warehousing….
NewsPress ReleasesPress Releases

Southwire Flexible Metal Conduit (FMC) from AutomationDirect

January 15, 2024 – AutomationDirect has added Southwire flexible metal conduit to their growing selection of electrical conduit and wiring solutions. Southwire’s Alflex™ type RWA (Reduced Wall Aluminum) and Galflex™ type RWS (Reduced Wall Steel) conduits are built using a metal strip that is helically formed into a continuously interlocked flexible metal conduit which can…
NewsPress ReleasesPress Releases

Penn-Union Compression Lugs and Crimp Tools from AutomationDirect

January 15, 2025 – AutomationDirect has added Penn-Union compression lugs to provide a secure method of terminating electrical cables, especially high-power or large-diameter cables, to electrical equipment. Unlike mechanical lugs, that are screwed/clamped in place, these connectors are crimped onto the cable using the appropriate crimping tool for a permanent installation. These connectors are rated…
IdentificationIssue 54 - 2025Notebook Issue

Industrial Strength Identification is Essential for Manufacturing

Applying the right barcode, RFID, and vision technologies addresses the increasing demand for data-driven manufacturing, improved quality control, and compliance with track-and-trace requirements. By Larry Reynolds, AutomationDirect Automation systems routinely use a variety of sensors to detect the position, motion, weight, and many other physical characteristics of products and other targets. This type of monitoring…
Motion ControlProduct

What is Industrial Servo Control?

Servo motors and drives use feedback to provide accurate position, speed, and acceleration control, making them ideal for demanding machinery and robotics applications. By Chip McDaniel, AutomationDirect Servo motor systems are a high-performance motion control technology, able to execute complex motion profiles while delivering high torque output, beyond the capabilities of typical direct current (DC)…
Issue 54 - 2025NewsNotebook IssuePress ReleasesPress Releases

Advantech Gateways & Ziplink Connector from AutomationDirect

December 18, 2024 – AutomationDirect has added Advantech serial-to-Ethernet Modbus gateways allowing connections of isolated serial devices to the Internet for centralized machine communication management. Advantech Modbus gateways provide easy integration of Modbus TCP and Modbus RTU/ASCII networks and offer two 10/100 Mbps Ethernet ports for LAN redundancy. These gateways can be set up and…
Issue 54 - 2025NewsNotebook IssuePress ReleasesPress Releases

Endress+Hauser Soliphant® FTM20 Vibration Rod Level Switches from AutomationDirect

December 18, 2024 – AutomationDirect has added Endress+Hauser Soliphant vibration rod level switches to detect fine- or coarse-grained, non-fluidized bulk solids in silos, hoppers, and bins. They can even detect solids underwater, such as sediment buildup in a tank. These robust switches are insensitive to buildup, providing maintenance-free operation and easy setup with no calibration required….
Issue 55, 2025NewsNotebook IssuePress ReleasesPress Releases

Captron CANEO Series Pushbuttons from AutomationDirect

December 18, 2024 – AutomationDirect has added more Captron capacitive pushbuttons that utilize touch control and are activated without pressure when a hand or body part nears the device’s surface. They feature a robust IP69K design, wear-free operation, resistance to water, oil, and harsh environments, and are available in various mounting/operator sizes. Caneo Series10 additions…
Issue 54 - 2025Issue 55, 2025NewsNotebook IssuePress ReleasesPress Releases

Lika Electronic Medium Duty Encoders and Encoder Linear Measuring Wheel Systems from AutomationDirect

December 18, 2024 – AutomationDirect has added four new series of Lika Electronic rotary encoders each with unique features or applications. Linear measuring wheel encoders are also now available. The new A41 series are compact (41mm diameter body) medium duty encoders with hollow or solid shafts and resolutions from 100 to 3600 PPR. A50 series…
NewsletterNewsletter

Newsletter Volume 26 Issue 12

Simplified Motion Control High-performance servo motion is now more affordable and accessible than ever due to integrated controllers, making the technology viable even for applications which could not formerly support the cost or complexity of traditional implementations. Learn more Turning Up the Heat on a Balky Boiler Applying commercial off-the-shelf automation products can provide the…
NewsletterNewsletter

Newsletter Volume 26 Issue 11

3-Axis Motion Made Simple in 3 Ways using CLICK PLUS PLCs | White Paper AutomationDirect CLICK PLUS PLCs, when combined with stepper motors, make advanced motion control and edge integration simple for smaller systems. Electric motors provide the motive force for many types of machinery and equipment. Sometimes standard AC and DC motors are operated…
NewsPress ReleasesPress Releases

Teknokol Eco Series HMI Enclosures and Suspension Arm Systems from AutomationDirect

December 11, 2024 – AutomationDirect has added Teknokol Eco series HMI enclosures and suspension arm systems which are designed to work together to provide customized, adjustable HMI panels using a selection of components and cut-to-length arm profiles. These suspension systems allow the HMI to be relocated as needed for better HMI visibility and operator comfort. …
Issue 54 - 2025NewsNotebook IssuePress ReleasesPress Releases

Murrelektronik EtherCAT® IO-Link Line Master Modules and Additional Io-Link Hubs from AutomationDirect

December 11, 2024 – AutomationDirect has added Murrelektronik Premium EtherCAT IO-Link master modules to their IO-Link product lineup. IO-Link masters provide standardized, point-to-point connections between smart devices and controllers. IO-Link functions similarly to traditional field I/O but adds the capability to collect diagnostic and operational data from IO-Link capable devices, helping pinpoint potential problems or…
Learning ResourcesUncategorizedWhite PapersWhitepapers

What’s Really Causing your VFD’s DC Bus Overvoltage Fault? | White Paper

Variable Frequency Drives (VFDs) are a crucial component in industrial automation, providing precise control over a motor’s speed and torque. Numerous built-in protections and fault indications are provided with modern VFDs, including the commonly seen DC Bus Overvoltage Fault. This fault has several possible causes and this whitepaper explores each one, offering solutions to ensure…
Issue 54 - 2025NewsNotebook IssuePress Releases

More NIDEC US Motors ACCU-Torq Motors from AutomationDirect

December 4, 2024 – AutomationDirect has added more ACCU-Torq motors from Nidec U.S. Motors. The ACCU-Torq motors are high-performance inverter duty motors and are an excellent cost-effective solution for applications that require 100% torque down to zero speed. They are available in 230/460 VAC and are now offered in sizes up to 20 hp at…
NewsPress ReleasesPress Releases

Helukabel SOOW & SJOOW Portable Cord from AutomationDirect

December 4, 2024 – AutomationDirect has added high quality Helukabel unshielded “extra hard use” 600V SOOW and 300V SJOOW portable cord. Portable cord (also called service cord) is cable with multiple conductors used for electrical power connections that are not intended to be permanent. Applications for these cables often involve portable equipment such as power tools…
Uncategorized

AC Drives—The Master Controller of Motors

Everyone knows that motors are the workhorses of industry. They move machinery, fans, pumps, compressors, conveyors, elevators, etc. How are they controlled? The simple way is by using across-the-line control and turning them on and off. This works great in most cases, but what if you need to vary the speed of the motor? Control…
NewsPress ReleasesPress Releases

Schneider Electric Easy TeSys Series IEC Motor Controls from AutomationDirect

November 20, 2024 – AutomationDirect has added Schneider Electric Easy TeSys series manual motor protectors, contactors, thermal overload relays, and accessories to their lineup of motor control products.  Schneider Electric Easy TeSys series IEC manual motor protectors are compact, easy to use, and cover the functions of disconnect, controller, thermal overload relay, and branch circuit…
NewsPress ReleasesPress Releases

FTG Enclosed Style Power Distribution and Terminal Blocks from AutomationDirect

November 20, 2024 – AutomationDirect has added FTG enclosed-style power distribution and terminal blocks to provide a convenient central location to connect several wires and distribute power from a single source to multiple loads. The enclosed power distribution blocks feature a modular design for easy multi-pole assembly and an IP20 finger-safe protection rating. They are…
Uncategorized

Issue 53, 2024

Welcome to the fall issue of AutomationDirect’s NOTEBOOK, your guide to practical products, technologies, and applications! This fall season has been difficult for many of us in the direct path of Hurricanes Helene and Milton. Our thoughts are with everyone personally impacted. From a business standpoint, AutomationDirect is paying close attention to the supply chain…
Issue 53, 2024Motion ControlNotebook IssueProductProgrammable Control

Build Better Machines Faster Using Today’s Enhanced Motion Controllers and PLCs

Process-enabled motion controllers and motion-enabled PLCs give OEMs the flexibility to optimize design and performance. By: Kevin McClelion and Joe Scoccimaro, AutomationDirect There was a time when designing machines that included motion control followed a standard architecture. The PLC handled basic machine control and a dedicated motion controller managed the motion axes. Today, the trend…
Application StoriesDistribution/LogisticsHMIIndustryOperator InterfacePLCProductProgrammable Control

Automating a Luxury Bus

Industrial automation products are useful for much more than traditional applications, as PLCs and HMIs can be used in all sorts of unique commercial markets. Byline: Mark McHenry, Systems & Controls Other than being large and generally rectangular-shaped, a modern custom bus—the type frequented by touring music stars, mobile multi-millionaires, and campaigning politicians—bears little resemblance…
Issue 53, 2024Motion ControlNotebook IssueProductProgrammable Control

Enhancing Automation System Performance with the EtherCAT Protocol

The EtherCAT protocol is a high-performance and cost-effective Ethernet networking technology, providing a versatile solution when EtherNet/IP and PROFINET simply aren’t fast enough. By Joe Kimbrell, AutomationDirect Ethernet rapidly expanded into and throughout commercial information technology (IT) networking connectivity environments beginning in the 1980s, and it has experienced rapid performance advancements and adoption since then…
Company TopicsIssue 53, 2024News

How Industrial Enterprises Can Address the “Grey Tsunami” Behind Today’s Growing Skills Shortage

By Chip McDaniel, Automation Expert & Education Specialist, AutomationDirect Human resources departments call the phenomenon the “grey tsunami.” They’re referencing an historic U.S. retirement surge of 4.1 million Americans a year. Manufacturing, in particular, is taking a big hit as industrial engineers, equipment operators, maintenance and repair technicians, plant managers, and others in supporting roles…
Company TopicsIssue 53, 2024NewsNotebook Issue

SIDirect: AutomationDirect’s Systems Integrator Program

The SIDirect program connects end users of all sizes with systems integrators ready to support their automation needs, spanning a variety of technologies and processes. By: Jeff Payne, AutomationDirect Every manufacturing business must make choices about supporting their machines, production processes, and personnel. Careful application of the right automation technologies and skillsets in each of…
AutomationDirect SpotlightIssue 53, 2024Notebook IssueStudent SpotlightStudent Spotlight

Industry Supports Rocket Science

Industrial-grade products provide a path for this student organization to develop a space-capable rocket. Byline: Oleg Khalimonov, Space Concordia Many are familiar with the phrase “it isn’t rocket science.” But today more than ever, sometimes it is rocket science. SpaceX and other organizations have made rocket launches and space exploration commercially viable and almost commonplace,…
Discrete SensingIssue 53, 2024Motion ControlNotebook IssueProcess Sensing & ControlProduct

What is an Encoder?

For determining the precise motion of industrial machinery and equipment elements, or servo motors, encoders provide a high-performance solution—but only if they are specified properly. By Joe Kimbrell, AutomationDirect Mechanical movement generated on automated machinery and equipment almost always needs to be monitored by sensors to provide a robust motion control solution. This is especially…
Issue 53, 2024Notebook Issue

Brainteasers - Issue 53, 2024

Truffle Kerfuffle The factory’s robotic truffle picker is making gift boxes with a single row of seven unique types of truffles. The assortment includes three white chocolate truffles, while the other four are milk or dark chocolate. The placement of the seven truffles in the row is completely random.  What are the odds that a…