ProSense Digital Panel Meters from AutomationDirect
NewsPress ReleasesPress Releases

ProSense Digital Panel Meters from AutomationDirect

AutomationDirect ProSense® digital panel meters in 1/32 and 1/8 DIN sizes are AC or DC powered and feature IP65-rated meter faces, simple menu-driven pushbutton configuration, and accept a wide variety of input signals. Available outputs include alarm relays, milliamp current, and sensor excitation voltage options. New process-display options now include (depending on series) AC or…
AutomationDirect adds Schmersal IP69K Rated Joysticks
NewsPress ReleasesPress Releases

AutomationDirect adds Schmersal IP69K Rated Joysticks

Schmersal joystick selector switches have design features that make them suitable for food processing, pharmaceutical, and medical applications. The joysticks comply with the special cleaning requirements of the food industry to prevent cross-contamination, particularly when used in machines that process raw goods. The IP69K rating also makes the joysticks suitable for marine applications, traffic systems,…
NITRA Rodless Air Cylinders from AutomationDirect
NewsPress ReleasesPress Releases

NITRA Rodless Air Cylinders from AutomationDirect

NITRA® L-Series Rodless Cylinders from AutomationDirect offer a robust design in a compact package. Rodless cylinders can offer the same stroke as rodded cylinders in a smaller space. Rodless cylinders have the piston connected to a carriage that rides outside the extruded cylinder wall, reducing overall length, making them ideal for small or tight location…
WEG Fully Digital Soft Starters and Micro VFD Drives from AutomationDirect
New ProductNewsPress ReleasesPress Releases

WEG Fully Digital Soft Starters and Micro VFD Drives from AutomationDirect

New compact soft starters and micro VFD drives have been added to the AutomationDirect motor controls lineup which encompasses simple manual controllers, motor contactors and starters, drives and soft starters. WEG SSW05 and SSW07 soft starters are compact, fully digital soft starters with state-of-the-art DSP (Digital Signal Processor) controller designed to provide great performance on…
Inductive Proximity Sensors with Analog Output from AutomationDirect
New ProductNewsPress ReleasesPress ReleasesUncategorized

Inductive Proximity Sensors with Analog Output from AutomationDirect

DW Series round metal inductive proximity sensors with analog outputs are now available from AutomationDirect in 8mm, 12mm, 18mm and 30mm cylindrical sizes. These reliable DC-powered (10-30V or 15-30V) threaded-barrel sensors are IP67 rated and are available with 2m pigtail cable or quick-disconnect. 8mm analog inductive proximity sensors detect the presence of ferrous metal objects…
ProSense Variable Area Mechanical Flow Meters from AutomationDirect
New ProductNewsPress ReleasesPress ReleasesUncategorized

ProSense Variable Area Mechanical Flow Meters from AutomationDirect

January 8, 2020 – ProSense® FG1 Series mechanical variable area flow meters provide visual indication of flow rate for water or petroleum-based fluids. These meters provide +/-5% full scale accuracy and a repeatability of +/-1%, important for cyclical applications requiring consistent readings. Two adjustable flow limit pointers are available to provide preset indication of high,…
Mele Kalikimaka from AutomationDirect!
Company TopicsNews

Mele Kalikimaka from AutomationDirect!

Relax, Reflect, Rejuvenate! Many of us take time off during this holiday season, but do we spend it wisely? Hopefully, on balance, we spend more time relaxing and enjoying our families, friends and faith, than running around or surfing to the next big sale for things we might use a few times and then forget….
Newsletter Volume 21, Issue 11
NewsNewsletterNewsletter

Newsletter Volume 21, Issue 11

Free HMI eBook AutomationDirect’s HMI Handbook delves into the world of human machine interfacing with informative chapters on selecting, designing and installing HMIs. But that’s just the first half, the back half of the book focuses specifically on C-more HMIs with chapters covering how to use screen objects, how to configure events, simulation basics, recipe…