IIoT projects should begin incrementally at the edge, using proven combinations of fieldbuses and controllers. Basic hardwired connectivity has long been typical for automation system designs. However, this approach is shifting as digital transformation and IIoT initiatives are expanding. InTech April 2023 features an article titled Field-Level Comms Improve IIoT Implementations, where Bill Dehner at…
Users are increasingly using AutomationDirect HMI, PLC, and router technologies to provide easy and secure industrial mobile access. Bill Dehner, technical marketing engineer for AutomationDirect, wrote an article for the November/December 2021 issue of Industrial Equipment News titled Evaluating Mobile Access Options. Here’s a summary, click on the link above for the full text. Using…
Programmable logic controllers (PLCs) are now gaining information technology (IT) abilities to interact directly with the internet, creating new automation and information possibilities. Bill Dehner, a Technical Marketing Manager at AutomationDirect, authored an article for the July 2019 issue of Control Engineering titled Benefits of Connecting a PLC to the Internet. Here’s a summary, click…
+Tech TopicsApplicationCommunicationsData and IIoTData System MonitoringeBookIIoT and DataLearning ResourcesOperator InterfaceProductWhy HMI
Layered Security Goes Beyond Hardware In IIoT Implementations
Industry is certainly starting to take note of the IIoT, which raises cybersecurity issues because it requires connecting field devices and other automation system components to the outside world, often through the internet. Connectivity capability is built into many automation components, typically via an Ethernet port, but can these connections be made secure?
ApplicationCommunicationsCompany TopicsData and IIoTData System MonitoringeBookIIoT and DataLearning ResourcesNewsProductProgrammable Control
Are You “Data-driven"? |Industry Survey
With all the talk lately about Big Data and the IIoT, we got to thinking about how much of an impact these trends would have on our industry. Since the primary goal of these two trends is to improve bottom lines/profit margins through data collection, data analysis and remote access, we were curious as to…
“The Industrial Internet of Things”…when you hear that term, what do you think? Now, some of you might be thinking, “Not another IIoT article!” or maybe, “I don’t need IIoT” or perhaps there are still a few of you that are wondering, “What is IIoT?” Well, when you get past all the buzz that is…
Automation NotebookData and IIoTeBookIIoT and DataLearning ResourcesOnline OnlyOperator InterfaceProductProgrammable Control
A Quick Look At Creating The IIoT
The IIoT starts with edge devices. Connecting these sensors, actuators, motors, drives and other smart devices to PLCs and other advanced controllers is the first step. The connection continues through the HMI to provide data sharing to both local and remote users through corporate intranets and the Internet. Connecting edge devices and distributing the data…
Many control systems these days need a way to interact with the process or machine operator. Legacy systems might present a whole panel full of pushbuttons, lights and switches; the development of electronic HMI (Human Machine Interface) devices made operator control and monitoring operations much more flexible, presenting text, graphics and even video to help…
+Tech TopicsApplicationCommunicationsCover StoriesData and IIoTData CollectionIIoT and DataIssue 33 - 2015Learning ResourcesMachine ControlNotebook IssueOperator InterfaceProductProgrammable Control
Linking Machines to IT Systems
Once upon a time, individual machines were stranded on an island, or just linked to other machines using a few discrete I/O and dry contact relays. Then came machine-to-machine data links such as a proprietary PLC-based network. Today, and certainly in the future, machines are being linked to IT systems.
If your company has remote sites that need to be monitored, and if you’re looking for a way to do this without making periodic rounds to check each site, then remote monitoring may be the answer. And if you’re looking for a cost effective yet powerful way to implement remote monitoring, embedded HMI is a…