January 15, 2024 – AutomationDirect has added Southwire flexible metal conduit to their growing selection of electrical conduit and wiring solutions. Southwire’s Alflex™ type RWA (Reduced Wall Aluminum) and Galflex™ type RWS (Reduced Wall Steel) conduits are built using a metal strip that is helically formed into a continuously interlocked flexible metal conduit which can withstand impact and crushing forces. Southwire’s Alflex type RWA and Galflex type RWS are designed for use with connectors intended for NEC Type FMC (Flexible Metal Conduit) and are REACH/RoHS-2 compliant.
Alflex type RWA is manufactured with a lightweight, high-strength aluminum alloy 66% lighter than steel and has superior corrosion resistance. Galflex type RWS is hot-dipped for a heavy zinc, rust/corrosion resistant coating.
Alflex type RWA flexible metal conduit coils start at $22.00, and Galflex type RWS flexible metal conduit coils start at $25.50.
Learn more by visiting: https://www.automationdirect.com/conduit-fmc
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo