AutomationDirect has expanded its Marathon AC motor line to include lower-cost, high-performance 0.5 to 5 HP Marathon Max+ series AC motors with integrated encoder. The 230/460 VAC Max+ inverter-duty motors are designed to replace 90 and 180 volt Permanent Magnet DC (PMDC) systems,
ApplicationApplication StoriesAutomation NotebookIndustryIssue 15 – 2009Learning ResourcesMachine ControlManufacturingMaterial HandlingNotebook IssueOperator InterfacePLCProductProgrammable ControlUser SolutionsVariable Speed Drives
Denim Manufacturer Upgrades Controls to Add Flexibility to Process Lines
Nestled along the Chatooga River, in Trion, Georgia, Mount Vernon Mills is one of the largest and oldest textile mills in the United States. Its long history dates back to 1845. The initial 5,000 square foot two-story mill had 40 employees and produced 5-lb. bunches of yarn to sell to local merchants from wagons. Over…
Automation NotebookBusiness NotesCompany TopicsIssue 2 – 2004Learning ResourcesNewsNotebook IssueProductVariable Speed Drives
Business Notes – Issue 2, 2004
RFID Will Affect Many Manufacturers And Packagers Radio frequency identification (RFID) has become one of the most visible issues in manufacturing and packaging in recent months. At its simplest, RFID is a generic term for technologies that use radio waves to automatically identify products to which a special tag has been affixed. To identify or…