• Home
  • Posts Tagged'Data Collection'

Posts Tagged ‘Data Collection’

Encoders Explained – Issue 25, 2013

What is an encoder?

An encoder (for industrial controls) is a special sensor that captures position information and relays that data to other devices. The position information can be read in many ways (optically, magnetically, capacitively, etc.). There are two …

Read more →
 

Gas Turbine Repurposed With PLCs – Issue 24, 2012

The Midwest Propulsion Group is a jet engine club dedicated to increasing the engineering knowledge and experience base of students by providing real-world engineering tasks related to gas turbine restoration and performance analysis, as well as finding vehicular applications for …

Read more →
 

Cellular Remote Access Gives Companies Competitive Edge

Internet and cellular technology make monitoring and control easier than ever.

The automation world, with its distant and often isolated sites, has long sought reliable remote access to cut costs and improve reliability. Instead of sending technicians to distant locations, …

Read more →
 

Advanced Automation, LLC Takes Baking To The Next Level – Issue 19, 2011

Advanced Automation, LLC, in Riverdale, New Jersey, is an automation systems manufacturing company specializing in creating solutions for companies in need of more efficient automated processes.

One such need is in the baking industry. Food associations, such as the British …

Read more →
 

PCA Provides Complete Turnkey, Cost-Effective Control System Solutions for a Variety of Industries – Issue 19, 2011

Pacific Coast Automation, Inc., located in Modesto, California, was founded in 2008 based upon the need for a competent, dependable and reasonably priced control system engineering firm, and not just a “controls tech” company which bases its existence on service …

Read more →
 

Top 10 Tips: Specifying VFDs (Part Two of a Two-Part Series) – Issue 21, 2011

This is part two of a two-part series on variable frequency drives. In Part One, we discussed how choosing the right variable frequency drive (VFD) can reduce energy consumption, improve realtime control, and lengthen motor life. Here are more expert …

Read more →
 

Top 10 Tips: Specifying VFDs (Part One of a Two-Part Series) – Issue 20, 2011

This is part one of a two-part series on variable frequency drives. VFDs can reduce energy consumption, improve real-time control, and lengthen motor life; selecting the right one for your application requires asking the correct questions. Here are some expert tips …

Read more →
 

Racing as Field Lab for Automotive Design – Issue 16, 2010

The University of Wisconsin Formula SAE team competes against over 130 universities from around the world in an annual competition held at Michigan International Speedway. The competition is based on the design and manufacture of a small scale open wheel, …

Read more →
 

M.M. & I., Inc Provides Production Information 24/7 To Pratt Industries – Issue 16, 2010

Michael Miles and Investors (M.M. & I.) has been in the commercial and industrial electrical markets since 1986. The company began by offering Web-based database and Visual Basic applications supporting school systems. In 1994, we ventured into the computer market, …

Read more →
 

Evolution of the ChemFreePro® Ion Generator – Issue 16, 2010

In the 1960s, NASA conducted a research program to develop a small lightweight water purifier. The purifier was for use in the Apollo spacecraft, so low power usage and minimal maintenance were a must. The 9-ounce purifier, slightly larger than …

Read more →
 
  • Page 1 of 2
  • 1
  • 2
© 2015 Library at AutomationDirect.com
Owned and Operated by AutomationDirect.com