May 29, 2024 – AutomationDirect now offers custom paint selections for Saginaw carbon steel Enviroline series single-door enclosures with ¼-turn latches. These enclosures can be custom-ordered with one of 15 color options in addition to the standard gray or light gray color. Custom paint options include graphite black, gentian blue, light blue, pebble gray, traffic…
An AutomationDirect product manager provides industrial enclosure selection essentials for Control Engineering readers. Industrial enclosures protect essential automation components that otherwise wouldn’t stand a chance in the face of harsh factory and field conditions. As automation technologies are trending toward more instrumentation and greater decentralization, the role of enclosures is adapting. Control Engineering interviewed AutomationDirect’s…
Here are basic steps for creating control panel designs. Chris Kregoski, product engineer for AutomationDirect, wrote an article posted in April 2022 on PanelBuilderUS.com titled Designing and Assembling Control Panels. Here’s a summary, click on the link above for the full text. Modern digitally controlled machines, equipment, and systems incorporate increasing numbers of smart devices…
There are a variety of solutions for heating, cooling, and dehumidifying electrical and control enclosure interiors to protect the components housed inside. While some electrical and electronic devices can be used unprotected in the field, most are installed within enclosures to protect them from the elements. Designers need to provide these enclosures with the right…
What is Needed for Industrial Control Panels? Industrial control panels are fundamental for protecting electrical, instrumentation, and control devices. The AutomationDirect portfolio of enclosures and components can help users obtain everything they need to create control panel solutions. Industrial control panels are commonly used for distributing power, housing pneumatics, and protecting automation electronics associated with…
Although we generally think of industrial enclosures as protecting components inside the box, it is also important to understand how they work with the environment outside the box. Jody Kinney, product manager at AutomationDirect, wrote an article for the July 2021 issue of Processing titled Thinking Inside and Outside the Box. Here’s a summary, click…
Specifying the right electrical enclosure protects personnel and equipment. Jim Krebs, Technical Marketing Engineer at AutomationDirect, wrote an article for the July 2020 issue of Processing titled Specifying the Right Electrical Enclosure. Here is a summary, click on the link above for the full text. Electrical enclosures are ubiquitous throughout public areas, buildings, and industrial…
Jim Krebs, technical marketing engineer at AutomationDirect, wrote an article in Processing magazine’s July 2018 issue titled Specifying Thermal Management Systems for Control Enclosures Most automation and electrical devices must be housed in a control enclosure when used in industrial environments. This includes controllers, drives, power supplies, disconnects, fuses, terminals, relays, contactors and more. Krebs…
Industrial facilities use many electrical enclosures to house automation and electrical components. Several of these enclosures require cooling and/or heating to control the climate within the enclosure to prevent condensation or component overheating. In this SlideShare, you will learn about the different types of climate control, reasons for use, and how to select and size…
On a walk around most any city, you’ll discover dozens of gray “boxes” that are fast becoming an ordinary part of the landscape. You can see these “boxes” attached to utility poles, along sidewalks, and near businesses and schools. Such “boxes” are really enclosures that protect wiring and electrical components vital to our ever-increasing automated…