Because AC motors are essential workhorses for industry, designers need to understand their applications to make detailed selections, such as single-phase or three-phase styles. Electric motors are a fundamental force for creating powered motion in any type of equipment. Initially developed in the 1800’s and refined significantly over the years, electric motors are now available…
Whether pumps are automated with hardwired controls or PLCs, designers can provide enhanced functional and protective features using control and monitoring relays. Lenny Filipkowski, Product Manager at AutomationDirect, wrote an article for the August 2021 edition of Process Instrumentation magazine titled Exploring Options for Process Pump Automation. Pump control is a common application used in…
Contactor Definition Contactors are a specialized form of relay capable of switching higher power loads such as motors, lighting and electric heaters. Turning large electrical power loads such as motors, lighting and heaters on and off is a common automation requirement. Applications are found in commercial buildings, industrial equipment and vehicles. The fundamental device for…
Automation systems must integrate multiple power and control subsystems and components into a coherent whole. Read on to learn more about machine automation basics. Chip McDaniel, who works in technical marketing for AutomationDirect, wrote an article for the Mar/Apr 2019 issue of InTech magazine titled Machine Automation Basics. In the article, he first lays out…
Learning ResourcesMachine ControlMotor ControlsOnline BlogProductProgrammable ControlVariable Speed Drives
Programming and Setup Considerations for VFDs with Integrated PLCs
Control capability built-in to VFDs are moving machine intelligence to the edge. Jeff Payne, Product Manager for AutomationDirect, wrote an article for the March 2019 issue of Design World, titled VFDs with integrated PLCs for motion and machine controls: Programming and setup considerations. Payne explains how AC drives can be controlled by either an external…
ApplicationApplication StoriesCompany TopicsEntertainmentIndustryLearning ResourcesMachine ControlMotor ControlsNewsOnline BlogPLCProductProgrammable Control
Let’s Ride the Roller Coaster! - An AutomationDirect Case Study
Manny Salazar, the Manager at Automated Integration LLC, wrote an article titled Roller Coaster Overhaul for the April 2018 issue of Automation World. The article told the story on how Automated Integration replaced an old PLC, a bunch of relays and what seemed like miles of wire when upgrading the control and safety system on…
Most automatic controls involve AC motor control in some way, especially in factory automation. Applications such as pumps, fans, robotics, and conveyors use motors. Whether general-purpose 3-phase ac motors, which are great for simple on/off systems, or the inverter-duty motors specifically designed for operation with variable frequency drives (VFDs), one could say that motors are ubiquitous…
General purpose motors have been around for many years. They are the workhorse of almost every industry. An inverter-duty motor is a much newer concept that became necessary as motors began to be driven by VFDs (inverters or AC drives). An inverter duty motor can withstand the higher voltage spikes produced by all VFDs (amplified…
What may seem to be a simple task of selecting a soft starter for your motor may be a more demanding task than first meets the eye. “I just need to know the HP and Voltage to pick the correct one, isn’t that right?”
AutomationDirect SpotlightMotor ControlsProductSupplier ProfilesSupplier ProfilesVariable Speed Drives
WEG| Small Town Touch with a Global Reach
It’s not every day that a 92-year-old founder of a global company comes to a sales meeting but that’s not unusual at WEG. This type of corporate culture defines the company and makes its customers eager to work with them. Whether it’s hosting backyard barbeques with executives or working side-by-side in the office, WEG has…