Recent Posts

CommunicationsIssue 60 - 2026Notebook IssueProductUncategorized

Designing Secure and Effective Industrial Control Networks

The IT/OT convergence is inescapable in the modern industrial market. Here’s how to optimize performance while maintaining a secure network. By: Damon Purvis, Alexander Maercz, and Winn Paulk; AutomationDirect For decades, the operational technology (OT) networks responsible for industrial controls were kept separate from IT networks. The approach protected critical industrial operations from vulnerabilities introduced…
Application StoriesDrivesHMIIssue 60 - 2026Notebook IssueOperator InterfacePLCProductProgrammable ControlVariable Speed Drives

Supporting Small and Specialized Automation Applications

How a small system integrator relies on proven automation products to reliably and responsively serve clients. Byline: Mike Watkins, AutoWorks Like enterprises in almost any sector of the economy, industrial automation systems integrators (SIs) come in a wide range of sizes. Many designers and developers, myself included, have worked at a few operations both small…
Application StoriesHMIIssue 60 - 2026Notebook IssueOperator InterfacePLCProductProgrammable Control

A Hands-On Home for Automation Learning

How a main-street innovation center is helping small-town utilities, students, and researchers get comfortable with industrial controls. By: Greg Martz, CoStream Small municipal water and wastewater systems are among the quietest success stories in American infrastructure. Some estimates suggest that about 90% of the water systems in the United States fall into the “small” category,…
Issue 60 - 2026Notebook Issue

Brainteasers Issue 60, 2026

Incessant Crescent Determine the area of the green shaded portion of the diagram, given only the lengths of the three chords on the major axes of the larger circle. Demonic Ultrasonics Twelve di-soric® Ultrasonic Proximity Sensors have been laid out in a familiar “3-4-5” triangular pattern, such that the bounded area of the right triangle…
NewsPress ReleasesPress Releases

Ashcroft T4 Series Mechanical Temperature Switches

August 5, 2026 – AutomationDirect now offers Ashcroft T4 series mechanical temperature switches which provide reliable temperature monitoring and control for demanding industrial applications. These rugged switches feature high 15A SPDT switch contacts that can directly control larger loads, reducing or eliminating the need for external contactors or interposing relays. The T4 series offers field-adjustable…
NewsPress ReleasesPress Releases

Gefran GRM-H Series Power Controllers

August 5, 2026 – AutomationDirect has added Gefran GRM-H series SCR power controllers that convert analog signals (0–10 V, 4–20 mA), PWM duty-cycle outputs, potentiometer, and discrete ON/OFF commands from PLCs and PID controllers into precise SCR-based control of AC power for industrial heating applications. These ultra-compact controllers are available in 10 A, 25 A,…
NewsPress ReleasesPress Releases

WERMA MC Beacons

August 5, 2026 – AutomationDirect has added WERMA MC beacons which deliver compact, high‑visibility status indication for machines and control panels, combining flexible LED signaling with rugged industrial design. This expanded offering includes 35mm and 55mm panel‑mount beacons, RYG (red, yellow, green) models, multicolor RGB units with up to seven selectable colors, and touch‑enabled variants…
AutomationDirect SpotlightSupplier ProfilesSupplier Profiles

Supplier Profile: GC Valves

Chances are, when you go to the car wash, you don’t think about the soap and wax metering systems or the low-pressure function controls that work to get your vehicle sparkling clean. In fact, a wide range of industrial and commercial applications rely on equipment behind the scenes to precisely control the flow of liquids…
NewsNewsletterNewsletter

Newsletter Volume 28 Issue 7

Tech Advancements Make Motion Control More Accessible Advances in motion control technology are making high-performance automation more affordable and easier to implement. Improved servo, stepper, and networked control solutions are reducing complexity while expanding application possibilities. Learn more Painlessly Connect OT with IT Using Industrial Edge Switches Industrial edge switches are helping bridge the gap between…
AutomationDirect SpotlightSupplier ProfilesSupplier Profiles

Supplier Profile: Sifam Tinsley

Demanding industrial environments call for panel meters that give clear, reliable readings, and Sifam Tinsley Instrumentation Inc. has answered that call. Along the way, the company has also developed solutions for every level of industrial electrical monitoring, becoming a global provider of electrical measurement and process control products. Its history is closely tied to the…
ProductSafety

Z-Range Safety Switch System

Simple. Intelligent. Modular. Scalable Safety, Simplified WiringThe Z-Range Safety Switch System delivers a flexible approach to machine safety that’s designed for modular machinery. Up to 30 devices can be connected in series to a single safety relay while preserving PLe and SIL 3 ratings, making it ideal for scalable systems. With built-in diagnostics and easy…
NewsPress ReleasesPress Releases

WAGO 207 Series Gelboxes and Additional Splicing Connectors

July 21,2026 – AutomationDirect has added WAGO 207 series gelboxes that deliver reliable, maintenance-free moisture protection for electrical connections in some of the toughest environments. Engineered for compatibility with WAGO’s 221 series LEVER-NUTS® and 2773 series PUSHWIRE® connectors, these compact enclosures are filled with a specialized silicone-free sealing gel that fully encapsulates conductors, providing IPX8-rated…
NewsPress ReleasesPress Releases

Lika Electronic Linear Encoders

July 21, 2026 – AutomationDirect has added Lika Electronic linear encoders that combine a sliding encoder body and a magnetically coded strip to provide extremely accurate linear position detection over distances up to 20 meters. A quadrature output results in accuracy up to 0.01mm, with single-increment repeatability (0.01mm/count) at speeds up to 20 m/s.  AME95 series…
NewsPress ReleasesPress Releases

Fuji Electric TK-E02 Overload Relays

July 15, 2026 – AutomationDirect now offers Fuji Electric TK‑E02 series thermal overload relays that expand the TK‑E lineup with compact, high‑precision protection for smaller motors and lower current applications. Designed to safeguard motor windings from overloads, locked-rotor conditions, and damaging open‑phase faults, the TK‑E02 delivers reliable performance in demanding motor control applications.  These relays…
NewsPress ReleasesPress ReleasesUncategorized

More STRIDE PRO Unmanaged+ Ethernet Switches

July 15, 2026-AutomationDirect has added more STRIDE PRO Unmanaged+ industrial Ethernet switches which are a step up from basic unmanaged switches, adding efficient network optimization with IGMP snooping (traffic prioritization), port monitoring, port alarms, VLAN support, and more. IGMP snooping ends network flooding by transmitting data only to the specific devices requiring it. Port mirroring…
NewsPress ReleasesPress Releases

Lapp ÖLFLEX 1XL VFD Cable

July 15th, 2026 – AutomationDirect now offers Lapp ÖLFLEX® VFD 1XL cable which delivers advanced performance for modern variable-frequency drive applications, helping overcome challenges caused by pulse-width modulation (PWM), including electromagnetic interference (EMI), motor stress, and reduced cable life. Engineered with cross-linked polyethylene (XLPE Plus) insulation and fine-stranded tinned copper conductors, this cable offers excellent…
Uncategorized

Motion Starts with What Moves It 

Every operation has one machine everyone depends on, the conveyor that never seems to stop, the gantry that positions with precision, the drive system that quietly powers everything behind the scenes. Over time, it becomes clear that even the most advanced systems rely on something simpler: the components that transfer motion.  At first, those components are easy…
NewsPress ReleasesPress Releases

More Murrelektronik Exact 12 Passive Distribution Blocks

July 1, 2026 – AutomationDirect has added more Murrelektronik Exact 12 passive distribution blocks that deliver a smarter, more efficient way to connect sensors and actuators and eliminate error-prone individual wiring in a compact, centralized solution. Designed for demanding industrial environments, they feature a space-saving 30 mm footprint, rugged overmolded construction for superior vibration and…
NewsPress ReleasesPress Releases

Murrelektronik M8 and M12 A-coded Sensor/Signal and Drag Chain Cables

July 1, 2026 – AutomationDirect has added more M8 and M12 4‑pin A‑coded sensor and signal cables which are designed to connect devices that use different connector sizes while maintaining standard 4‑pin wiring, helping eliminate rewiring, reduce installation time, and minimize common wiring errors. They are well-suited for applications across automotive manufacturing, food and beverage…
ProductSafetyWhite Papers

Selecting Safety Components Properly | White Paper

Facility, system, and machinery safety are important factors to prevent injury and loss of productivity in the workplace. Safety component ratings ensure that the proper device is selected for your application. Understanding these ratings will make this decision much easier. Table of Contents
NewsletterNewsletter

Newsletter Volume 28 Issue 6

Taming Ladder Logic with Object-Oriented Techniques Programmable logic controllers (PLCs), prized for their ruggedness and real-time performance, have formed the industrial automation backbone of operational technology (OT) systems since the late 1960s. While traditional PLC programming methods were historically less sophisticated than solutions developed for the information technology (IT) industry, the situation has been steadily…
NewsPress ReleasesPress Releases

ABB - Thomas & Betts Cable Ties and Cable Tie Tools

June 24, 2026-AutomationDirect has added ABB-Thomas & Betts cable management solutions that combine durability, efficiency, and ease of installation, with Ty‑Rap® stainless steel tooth cable ties, Ty‑Grip® reusable cable ties, and dedicated cable tie installation tools. Ty‑Rap cable ties are engineered for secure, long‑term bundling, using a hardened stainless steel locking tooth and UL‑rated Nylon…
NewsPress ReleasesPress Releases

RECOM Power RACPRO1 Series Single-Phase Switching Power Supplies

June 24, 2026 – AutomationDirect has added RECOM Power RACPRO1 series single-phase DC power supplies which are a highly reliable, low-cost solution for harsh industrial automation and renewable energy applications. These power supplies include adjustable power outputs and other model-specific features, including selectable power boost, switchable constant current or parallel mode, and a load LED display…
NewsPress ReleasesPress Releases

More I/O Modules for the Productivity2000 PLC Series and New Productivity Suite Software Features

June 24, 2026 – AutomationDirect has added more I/O modules for the Productivity2000 PLC series. New combination I/O modules deliver increased flexibility and efficiency by integrating multiple input and output points into a compact footprint, helping reduce both panel space and overall system cost. Available options include DC input modules paired with sinking or sourcing…
NewsPress ReleasesPress Releases

Wachendorff IP69K Rotary Encoders and Measuring Wheel Components

June 24, 2026-AutomationDirect now offers Wachendorff 58V and 36J series encoders that sport both IP67 and IP69K ratings, making them well-suited for high-pressure, high-temperature, washdown environments. IP69K is essential for sanitation compliance and protects against dust and intense, close-range liquid jets, including those used for high-pressure steam cleaning. The 58V models have additional resistance to acidic…
NewsPress ReleasesPress Releases

WAGO Base Series Single-Phase Power Supplies

June 17th, 2026-AutomationDirect now offers WAGO Base series single-phase switching power supplies that combine a slim form factor with regulated DC outputs, providing low-cost, safe, and reliable power that is ideal for space-limited enclosures. These power supplies offer easy 35mm DIN rail installation, quick wiring with their convenient, tool-free, push-in termination connectors, a wide 90-264 VAC…
NewsPress ReleasesPress ReleasesUncategorized

Cembre Knockouts & Punching Tools

June 17, 2026-AutomationDirect’s lineup of knockout and punching tools now includes Cembre hydraulic knockout punching tools and accessories that deliver fast, clean, and accurate cutouts in steel, stainless steel, fiberglass, and plastic sheet materials—eliminating the need for any secondary finishing. A puller‑type hydraulic mechanism applies consistent force through the entire punch stroke, producing smooth, burr‑free…
NewsPress ReleasesPress Releases

Atkore Stainless Steel Hygienic Connectors

June 10, 2026-AutomationDirect has added Atkore stainless steel hygienic straight and 90° connectors that are designed to create secure, liquid-tight connections between hygienic flex conduit and metal enclosures in sanitary environments such as food and beverage or pharmaceutical facilities. Built from Type 316 stainless steel and equipped with FDA-grade sealing components, they support strict hygiene…
NewsPress ReleasesPress Releases

C-more CM5 V9.0 HMI Programming Software

June 10, 2026-AutomationDirect offers new C‑more® CM5 series programming software version 9.00 that delivers a faster, smarter HMI development experience. With up to 250% improved screen performance over previous versions and powerful new visualization tools like advanced line and step charts with dual Y‑axes and dynamic scaling, this software streamlines development and improves overall system…
NewsPress ReleasesPress Releases

Additional Crohm Brake Resistors

June 10, 2026-AutomationDirect now offers additional Crohm brake resistors that are designed and manufactured in the USA and feature rugged construction, industry-standard wattage/ohm combinations, and compatibility with drives up to 600 VAC.  The new additions include encapsulated flat mount PL-series models (from 200W to 500W) that provide compact, durable options ideal for installations where panel…
Issue 60 - 2026NewsNotebook IssuePress ReleasesPress Releases

Greenlee Knockout & Hydraulic Tools

June 10, 2026-AutomationDirect now offers Greenlee® knockout punches, hydraulic drivers, and accessories, providing even more ways to create clean, precise holes in a variety of materials without drilling or rework. The expanded selection covers manual, hydraulic, Quick Draw®, and cordless battery‑powered ram or driver options. Greenlee’s proven Slug-Buster® and standard round punch series are available…
NewsPress ReleasesPress Releases

Rockford Ball Screw (RBS) Ball Screws and Nuts

June 3, 2026-AutomationDirect now offers RBS ball screws and nuts to support precise linear motion in both OEM and maintenance replacement applications.  Designed to convert rotational motion into linear movement, these US-manufactured ball screws are engineered for high positioning accuracy, low friction, and long service life. Utilizing recirculating ball bearings that roll rather than slide, they…
Issue 60 - 2026NewsNotebook IssuePress ReleasesPress Releases

More METEcon Multi-Wire Connector Housings and Inserts

June 3, 2026 – AutomationDirect has added METEcon multi-wire connectors that simplify complex industrial wiring while improving long-term reliability. Our expanded offering includes more inserts, housing components (including new 32B size), and configuration options without increasing complexity. With pole configurations from 2 poles plus ground up to 108 poles plus ground, screw or crimp terminations,…
Issue 60 - 2026NewsNotebook IssuePress ReleasesPress Releases

Flodraulic Continental Hydraulic Valves

June 3, 2026 – AutomationDirect now offers Continental hydraulic valves which provide rugged, high‑performance control for industrial hydraulic systems built around NFPA standards. Available in D03 and D05 sizes, these valves support a wide range of circuit requirements while maintaining consistent operation under high pressure and demanding duty cycles. NFPA D03 solenoid valves deliver reliable,…
Content Collections

Safety Starts Before the Work Does

Every workplace has that one person who seems to notice what everyone else overlooks. In one small manufacturing facility, that person was Bryce, a maintenance supervisor who had a habit of stopping by workstations before shifts began—not to interrupt, but to ask a simple question: “Is everything ready to run safely today?” At first, those…
NewsletterNewsletter

Newsletter Volume 28 Issue 5

Modern PLCs Support Dependable SCADA Communications Water and wastewater treatment systems of all sizes are essential and roughly 90% of U.S. systems are considered small (serving 10,000 or fewer people). Though large and small plants often use similar technologies, they operate at very different scales and budgets for automation and staffing. Recognizing this disparity, the…
NewsPress ReleasesPress Releases

Gladiator DIN Rail Mounted Duplex Receptacles with USB Models

May 27, 2026 – AutomationDirect now offers more Gladiator GR series DIN rail mounted duplex receptacles that are convenience outlets easily installed within electrical enclosures to provide temporary power for laptop computers, test equipment, and USB powered devices. The new GR-REC2 model consists of two NEMA 5-15 straight blade receptacles, the GR-REC2-GFCI adds GFCI protection,…
CommunicationsProduct

Painlessly Connect OT with IT Using Industrial Edge Switches

Unmanaged+ industrial Ethernet switches apply key IT technologies—including VLANs, QoS, IGMP snooping, and more—in easily deployed OT-friendly hardware, all without any required complex management. Today’s manufacturers are pursuing data analytics, AI-driven optimization, remote support, and enterprise-wide visibility, which means that their operational technology (OT) networks can no longer remain isolated from information technology (IT) systems….
NewsPress ReleasesPress Releases

SJT Industries SIM Couplings and Timing Pulleys

May 20, 2026-AutomationDirect now offers a wide selection of SIM couplings, along with a new offering of 8M timing pulleys, which has been added to support reliable power transmission in both OEM and MRO applications. Designed for precise motion control, these components help efficiently transmit torque and rotational power between shafts and belt‑driven systems across…
NewsPress ReleasesPress Releases

Lapp OLFLEX 190 Flexible Control Cable

May 20, 2026-AutomationDirect has added Lapp OLFLEX® 190 flexible control cable which provides a new, rugged, versatile option for demanding industrial wiring applications. Designed for machinery, equipment, and control panels, OLFLEX 190 features finely stranded copper conductors with number‑coded insulation and an oil‑, coolant‑, and solvent‑resistant outer jacket for reliable performance in dry, damp, or wet locations….
+Tech TopicsIssue 59, 2026Learning ResourcesNotebook Issue

Industry 5.0: The Human-Centric Shift

By: Kristin Lewotsky, contributing writer Industry 4.0 is a conceptual framework that applies industrial networking, data-gathering and analytics, and smart devices to cut costs and boost efficiency. It emphasizes improving performance by automating processes and removing humans from the loop. Industry 4.0 led to substantial gains in productivity and profitability. It wasn’t universally applicable, however….
Uncategorized

Issue 59, 2026

Highlights For the last decade (or more), the manufacturing industry has been adopting Industry 4.0 technology. A mashup of the Internet of Things (IoT), network connectivity, cloud computing, analytics and 3D printing have formed the foundation of what’s been leading us toward widespread digital transformation. It’s been the ultimate automation experiment. Especially when we started…
Issue 59, 2026Notebook IssueProductVariable Speed Drives

Tech Advancements Make Motion Control More Accessible

Modern servo and stepper motors and drives—combined with innovations in controllers, communications, and software—have simplified motion control integration and multiplied the possibilities for applying these technologies. By Joe Kimbrell, AutomationDirect Early motion control applications developed a (mostly) well-deserved reputation for requiring costly and esoteric components and technologies that are complex to design, install, configure, and…
Application StoriesIssue 59, 2026Notebook IssuePLCProductProgrammable Control

Mixing Dairy Feed with Automation

Automating livestock feed mixing in an accessible way provides the ideal solution for dairy farmers. By Miles Brake, W.G. Dairy Supply, Inc. W. G. Dairy Supply, Inc. (W.G. Dairy) is an innovative equipment and services supplier in the agricultural space. A portfolio of mechanical and automated equipment, and the company’s ability to provide additional automation…
Application StoriesHMIIssue 59, 2026Notebook IssuePLCProductProgrammable Control

Lights, Camera, Automation!

An automation upgrade allowed a professional summer stock theatre company to integrate its lighting systems, improving control while simplifying operations. By Ryan Poethke, ShowFab In the theatre, lighting sets the stage—creating an atmosphere and evoking mood even before the actors appear. Behind the scenes, however, there is far more than meets the eye: a fascinating…
Application StoriesAutomationDirect SpotlightIssue 59, 2026Notebook IssuePLCStudent Spotlight

Mission Control Built on an Industrial Foundation

These engineering students relied on an industry-proven automation platform and other products, to rapidly create a reliable rocketry ground test system. Byline: Jayden Sorensen, Electrical Lead As rocket companies have advanced from using single-use, expendable rockets to now achieving landing and reuse of the vehicles, much of the cost of transporting people and payloads into…
+Tech TopicsIssue 59, 2026Learning ResourcesNotebook Issue

Easy EtherCAT Connectivity

While PROFINET and EtherNet/IP are among the most well-known industrial Ethernet communication protocols in North America, there are compelling reasons to choose EtherCAT for your next motion control or automation design. By Chip McDaniel, AutomationDirect For new industrial automation installations, as well as retrofits and upgrades, Ethernet adoption continues to grow as traditional fieldbus technology…
NewsPress ReleasesPress Releases

Saginaw NEMA 1 and Sanitary Enclosures with Various Accessories

May 13, 2026 – AutomationDirect has added Saginaw NEMA 1 wall‑mount enclosures which are designed for indoor use where economical, reliable protection is essential. Available in a wide range of sizes, these enclosures feature sturdy carbon steel construction, convenient knockouts on all sides for streamlined wiring, 180‑degree door opening for easy access, and compatibility with common…
NewsPress ReleasesPress Releases

Additional Metal Work Pneumatic and New Potable Water Components

May 13,2026 – AutomationDirect now offers additional Metal Work pneumatic and new potable water components that support both general and specialized applications. The BIT series air prep line includes compact, cost effective filters, coalescing filters, regulators, lubricators, filter regulators, and complete FRL units. Available in multiple pressure ranges with 1/8″ and 1/4″ NPT ports, select units…
NewsPress ReleasesPress Releases

Additional Stahl Zener Barriers and Isolators

May 13, 2026 – AutomationDirect now offers STAHL Zener barriers and intrinsically safe isolators expands our offering of safety products, further strengthening our ability to support a wide range of hazardous area applications.  This expanded lineup adds single- and multi-channel support for the following input signals: zero-potential contacts, vibration transducers, 7.5 VDC load cells, analog…
NewsPress ReleasesPress Releases

Enhanced Datalogic Safety Laser Scanners from AutomationDirect

May 6, 2026 – AutomationDirect now offers Datalogic series safety laser scanners in enhanced models, delivering advanced protection for machinery, robotic cells, and mobile automation applications. These next-generation scanners use time of flight measurement technology to safely monitor up to a 72 m² area with a wide 275° scanning angle, ensuring reliable detection in even…
NewsPress Releases

Hammond NEMA 1 Hinged Lay-in Wireways from AutomationDirect

May 6, 2026 – AutomationDirect now offers Hammond wireways which are designed to house electrical cables and wires, keep them organized, and protect them from environmental contaminants or physical damage. The new CW series carbon steel lay-in wireways are available with a NEMA 1 rating, a hinged screw cover, and are offered with or without…
Issue 59, 2026Notebook Issue

Brainteasers - Issue 59

Semi-Circular Logic A green simicirle is inscribed inside a right triangle as shown.  What is the area of the semicircle? Brainwasher Find the areas of the two annuli (green shaded “washers”) in the figure below (hint: they have the same area). Checkmate Can you cut the pattern shown into exactly 2 pieces and reassemble them…
NewsletterNewsletter

Newsletter Volume 28 Issue 4

Five Ways AI Will Grow ROI on Plant Floors in 2026 AI isn’t new to manufacturing. Vision systems can already spot defects; predictive maintenance models can keep bearings from failing unexpectedly; and scheduling software can adjust production on the fly. What’s changing in 2026 is the reach and capabilities of these tools as well as…
NewsPress ReleasesPress Releases

Autonics CT Series Counter/Timers from AutomationDirect

April 29, 2026 – AutomationDirect now offers Autonics CT series counter/timers that deliver a powerful, easy-to-use solution for counting, timing, and batching applications, backed by the trusted Autonics brand. Designed for fast setup, these versatile units can be configured directly from the front-panel pushbuttons, with select models programmed via RS 485 using Autonics DAQMaster software….
Issue 60 - 2026NewsNotebook IssuePress ReleasesPress Releases

Mindman Pneumatic Valves from AutomationDirect

April 29, 2026 – AutomationDirect has added Mindman MVSC and MVSC1 directional control solenoid valves and manifolds which provide reliable, high performance air control for a wide range of automated systems. The MVDC stackable solenoid valve series builds on that capability with a modular design that keeps installations clean and scalable, making it easy to…
NewsPress ReleasesPress Releases

IronHorse ES1 AC Drives from AutomationDirect

April 29, 2026 – AutomationDirect now offers IronHorse ES1 AC drives that allow simple AC motor control for 3/4 up to 2 hp 230 VAC three-phase motors from a single-phase 120 VAC or 230 VAC input. These drives are proudly made in the USA and feature a simplified setup, requiring no software or parameters. The…
AutomationDirect SpotlightSupplier ProfilesSupplier Profiles

Supplier Profile: RuB Inc

Fluid control plays a critical role in everyday life. Gas, water, air, oil – they all need precise control to ensure comfort and safety at home and within an array of industries. Behind the scenes, one family-owned company has spent over seven decades engineering the valves that keep these important systems running. RuB Inc. is…
ProductProgrammable Control

Taming Ladder Logic with Object-Oriented Techniques

User-defined instructions are flexible and reusable blocks of code, useful for simplifying and speeding logic development. Programmable logic controllers (PLCs), prized for their ruggedness and real-time performance, have formed the industrial automation backbone of operational technology (OT) systems since the late 1960s. While traditional PLC programming methods were historically less sophisticated than solutions developed for…
NewsPress ReleasesPress Releases

Fandis Lumeis Enclosure Lights

April 22, 2026 – AutomationDirect has added Fandis Lumeis series LED enclosure lights that are designed to deliver powerful lighting performance, unmatched energy efficiency, and effortless installation. These lights provide 600 lumens of bright, uniform light while consuming less than 5 watts, making them an ideal solution for energy-conscious engineers and panel builders. The Lumeis…
NewsPress ReleasesPress Releases

Laumas Single Point Load Cells LE

April 22, 2026 – AutomationDirect now offers Laumas ALLUE, AZLUE, and APLUE series single‑point load cells that support industrial weighing applications from compact platform scales to larger conveyor and hopper systems. Manufactured in Europe to strict quality standards, this lineup provides scalable weighing options up to 600 kg (1320 lb). These models feature 0.02% full‑scale accuracy, a…
NewsPress ReleasesPress Releases

RHINO PSR Spring Clamp Power Supplies

April 22, 2026 – AutomationDirect has added RHINO PSR series power supplies with tool‑free spring clamp terminals provide secure, vibration‑resistant connections that never need retorquing, delivering long‑term reliability in industrial panels. These competitively priced power supplies combine an ultra‑slim design with rugged metal or aluminum housings, making them ideal for space‑constrained control cabinets. With high…
NewsPress ReleasesPress Releases

AchieVe NEC2 Power Supplies

April 22, 2026- AutomationDirect has added AchieVe PSA series NEC Class 2 power supplies that combine a compact form factor with energy-limited DC outputs, providing safe, reliable power for low-voltage control and automation circuits. Their competitive pricing and slim profile make them ideal for small control loads and space-limited enclosures. The power supplies feature a…
Application StoriesIndustryOperator InterfacePLCProductProgrammable ControlWater/Wastewater

Accessible Automation Helps Small Utilities Modernize Operations

A wastewater treatment utility is moving away from aging control hardware by replacing specialized components with easy-to-use programmable logic controllers. Like many small utilities throughout the country, the Harvest-Monrovia Water & Sewer Authority in Alabama was faced with supporting an aging mix of control technologies. Wesley Benefield of RTUDirect wrote this article for Automation.com April…
NewsPress ReleasesPress Releases

BLOCK Power Advanced Series Power Supplies with Battery Control / UPS and More

April 15, 2026 – AutomationDirect now offers BLOCK DC uninterrupted power supply (UPS) devices and modules which provide low-cost solutions for applications requiring continuous equipment operation. The Power Advanced series offers a switching power supply and a battery control module in one unit for optimal battery management, along with a UPS system to monitor the…
AutomationDirect SpotlightSupplier ProfilesSupplier Profiles

Supplier Profile: Penn Union

We all learned at an early age that electricity powers the world. The team behind Penn-Union learned how to harness that power, creating electrical connection solutions that perform even in some of the most challenging applications across industries such as commercial construction, utilities, data storage, telecom and aerospace. Founded in 1928, Penn-Union operates a fully…
NewsPress ReleasesPress Releases

New AchieVe Pressure Switches at AutomationDirect

April 1, 2026 – AutomationDirect now offers AchieVe LPPS and S18-1C mechanical pressure switches which deliver rugged, reliable pressure sensing for demanding industrial applications. Built with durable brass housings and simple, secure setpoint adjustment, these switches provide dependable relay outputs without the need for external contactors or interposing relays. The LPPS series supports pressure ranges…
NewsPress ReleasesPress Releases

Channellock Linesmans & Locking Pliers LX

April 1st, 2026-AutomationDirect has added CHANNELLOCK® American-made pliers and tool sets are engineered for tradespeople who demand reliability on every job. V-jaw pliers offer superior contact on pipes, tubing, and round stock thanks to their unique geometry. With laser-hardened teeth, PERMALOCK® fasteners, and a slip-resistant undercut tongue-and-groove design, these pliers deliver extreme holding power. For…
NewsPress ReleasesPress Releases

di-soric Ultrasonic Sensors

April 1st, 2026-AutomationDirect now offers di-soric 8, 12, 18, and 30mm tubular and 12mm rectangular ultrasonic proximity sensors that are designed for contactless distance measurement and offer IO-Link with ISDU support, a rugged nickle plated brass construction, high IP67 protection ratings, and sensing distances up to 6,000mm. ISDU (Indexed Service Data Unit) provides on-demand exchange…
Issue 60 - 2026NewsNotebook IssuePress ReleasesPress Releases

Ironhorse ACM AC Drives and ACN EtherCAT Communications Modules from AutomationDirect

March 25, 2026 – AutomationDirect has added IronHorse ACM Series AC drives provide basic V/Hz and sensorless vector control for low-horsepower motors when only single-phase power is available.  These VFDs accept a 120 VAC or 230 VAC single-phase power source and control motors from 1/8 to 3 horsepower. 5 digital inputs, 2 relay outputs, 2…
NewsPress ReleasesPress Releases

Shaviv Deburring Tools, Sets and Accessories from AutomationDirect

March 25, 2026 – AutomationDirect has added Shaviv deburring tool sets offer complete turnkey solutions for professionals who need multi-material capability right out of the box. The premium 21-piece (154-00024) and 12-piece sets (154-90085) feature ergonomic universal handles, extendable blade holders, and a comprehensive selection of rotating B- and E-series blades—ensuring you have the right…
NewsPress ReleasesPress Releases

Define Instruments Panel Meters & Signal Conditioners

March 25, 2026-AutomationDirect now offers Define Instruments digital panel meters, signal conditioners, and temperature transmitters that feature versatile measurement options and easy configuration. The Merlin series digital panel meters accept current, temperature, voltage, potentiometer, and pulse inputs and provide advanced scaling, linearization, and optional analog retransmission or relay outputs. A bright LED display, IP65 front…
Issue 60 - 2026NewsNotebook IssuePress ReleasesPress Releases

More Datalogic Smart-VS Vision Sensors from AutomationDirect

March 25, 2026-AutomationDirect now offer Datalogic Smart-VS vision sensor family models with expanded features. The new Smart-VS Plus sensor includes all the features of the standard Smart-VS sensor, including Ethernet communication and several I/O points, but adds additional object classifications for a total of 3 classes, which is useful when Good/No Good/No Object tests are…
NewsletterNewsletter

Newsletter Volume 28 Issue 3

Getting with the Object-Oriented Program Object-oriented programming concepts have become an important part of modern industrial automation, helping streamline PLC and HMI development. The introduction of user-defined instructions (UDIs) across the AutomationDirect Productivity PLC platform gives developers a new way to encapsulate logic and data. This approach accelerates development, promotes reuse of proven code, and…
NewsPress ReleasesPress Releases

RuB Manual Ball Valves from AutomationDirect

March 11, 2026 – AutomationDirect now offers RuB manual ball valves that bring unmatched versatility, performance, and reliability to fluid and air control applications. Featuring a lifetime warranty, the available offering spans everything from compact micro and mini valves, perfect for tight space OEM builds, to high flow industrial options engineered for demanding environments. General…