Robust real-time industrial control is essential, and remote connectivity is also becoming indispensable for many users. Here are some considerations for achieving the best of both worlds. Damon Purvis at AutomationDirect wrote an article for the February 2023 issue of Processing. Titled Balancing Local Automation with Remote Connectivity, this article explores some concepts around designing…
AgricultureApplicationApplication StoriesData CollectionData System MonitoringIndustryMachine ControlOperator InterfacePLCProcess ControlProductProgrammable ControlWater/Wastewater
SCADA Upgrade Provides Quick Compliance
Sensible Automation Solutions updated its customer to an AutomationDirect BRX Do-more PLC to add needed capabilities and data reporting to an existing wastewater treatment system.
The tried and true industrial data collection methods of the last several decades will expand into the future as Big Data and IIoT technology developments lead to more data, analytics and related benefits. Bill Dehner, Technical Marketing Engineer at AutomationDirect, wrote an article for the September-October issue of IEN titled Data-Driven Trends. Dehner says many…
+Tech TopicsApplicationCommunicationsCover StoriesData and IIoTData CollectionIIoT and DataIssue 33 - 2015Learning ResourcesMachine ControlNotebook IssueOperator InterfaceProductProgrammable Control
Linking Machines to IT Systems
Once upon a time, individual machines were stranded on an island, or just linked to other machines using a few discrete I/O and dry contact relays. Then came machine-to-machine data links such as a proprietary PLC-based network. Today, and certainly in the future, machines are being linked to IT systems.
ApplicationApplication StoriesAutomation NotebookAutomationDirect SpotlightData CollectionIndustryIssue 28 - 2014Learning ResourcesNotebook IssuePLCProcess ControlProductProgrammable ControlSystem IntegratorsUser SolutionsWater/Wastewater
An Affordable Retrofit Prevents Expensive Replacements
The Harvest-Monrovia Water & Sewer Authority (HMWSA) was established in August 1965 to operate and maintain a water system to provide domestic water in the Harvest-Monrovia area of Madison County, located near Huntsville, Alabama. In the early years, the utility serviced only 700 customers. As a result of growth in the area, the HMWSA now…
+Tech TopicsApplicationAutomation NotebookData CollectionIssue 28 - 2014Learning ResourcesNotebook IssueProductProgrammable ControlTechnology Brief
DataWorx with Do-more PLC support
AutomationDirect has partnered with BizWareDirect for several years, supplying DataWorx data collection and monitoring software for compatible DirectLOGIC programmable logic controllers (PLCs), Productivity3000 and WinPLC controllers. Previously, it had been necessary to purchase an OPC/DDE server and write code, or buy an HMI package, to collect data from AutomationDirect controllers. BizWareDirect’s data collection software makes…
ApplicationData and IIoTData CollectionIIoT and DataLearning ResourcesProductProgrammable ControlWhite PapersWhitepapers
PLCs & PACs Simplify Data Acquisition | White Paper
In today’s competitive market, companies need detailed and timely information about process variables, and production amounts, as well as alarms in real time. In the past, PLCs did not have the capabilities to provide such information, and PACs were not yet widely available. Fortunately, newer PLCs and PACs can perform many data acquisition tasks within…
ApplicationApplication StoriesAutomation NotebookAutomationDirect SpotlightData CollectionData System MonitoringEducation/DIYEnergy/UtilitiesHMIIndustryIssue 24 - 2012Learning ResourcesNotebook IssueOperator InterfacePLCProductProgrammable ControlStudent SpotlightStudent Spotlight
Gas Turbine Repurposed With PLCs
The Midwest Propulsion Group is a jet engine club dedicated to increasing the engineering knowledge and experience base of students by providing real-world engineering tasks related to gas turbine restoration and performance analysis, as well as finding vehicular applications for such engines.
+Tech TopicsApplicationApplication StoriesAutomation NotebookData and IIoTData CollectionData System MonitoringFeature StoryHMIIIoT and DataIssue 22 – 2012Learning ResourcesNotebook IssueOperator InterfaceProduct
Cellular Remote Access Gives Companies Competitive Edge
Internet and cellular technology make monitoring and control easier than ever. The automation world, with its distant and often isolated sites, has long sought reliable remote access to cut costs and improve reliability. Instead of sending technicians to distant locations, operators can now access critical information and control systems quickly and easily.
ApplicationApplication StoriesAutomation NotebookAutomationDirect SpotlightData CollectionIssue 19 – 2011Learning ResourcesMachine ControlNotebook IssueOperator InterfaceProductProgrammable ControlSIDirectSystem IntegratorsVariable Speed Drives
PCA Provides Complete Turnkey, Cost-Effective Control System Solutions for a Variety of Industries
Pacific Coast Automation, Inc., located in Modesto, California, was founded in 2008 based upon the need for a competent, dependable and reasonably priced control system engineering firm, and not just a “controls tech” company which bases its existence on service calls. Since its meager beginning, PCA has seen an almost 500% growth from 2009 to…