This utility standardized and defined best practices for their applications, improving operations while saving time and money. By David Reagan, Helix Water District ndustrial automation installations come in many shapes and sizes. Applications vary from standalone machines up to large processes, and the operating organization may have just one maintenance person or field an entire…
See how a water utility standardized around AutomationDirect products to improve operations while saving time and money. A team of operations, maintenance, and engineering personnel at Helix Water District in San Diego, CA has retrofitted and constructed many sites using automation hardware and best practices based on AutomationDirect products. David Reagan wrote an article with…
AgricultureApplicationApplication StoriesData CollectionData System MonitoringIndustryMachine ControlOperator InterfacePLCProcess ControlProductProgrammable ControlWater/Wastewater
SCADA Upgrade Provides Quick Compliance
Sensible Automation Solutions updated its customer to an AutomationDirect BRX Do-more PLC to add needed capabilities and data reporting to an existing wastewater treatment system.
Gary H. Lucas, Director of Innovation at Innovative Treatment Products, wrote an article that ran in the July 2018 issue of Control Design magazine titled Wastewater Treatment Plants Can Be Built for Small-Scale Applications. Any facility too isolated to connect to a larger sewer system—such as a school, office or retailer—will have to supply its…
ApplicationApplication StoriesAutomation NotebookAutomationDirect SpotlightData System MonitoringEducation/DIYIndustryIssue 34 - 2016Learning ResourcesMotion ControlNotebook IssueOnline OnlyOperator InterfacePLCPLC eBookProductProgrammable ControlStudent SpotlightStudent SpotlightWater/Wastewater
Portable Water Treatment Platform Removes Phosphorus Economically
A trailer-mounted water treatment process controlled by a Productivity2000 PLC has recently been developed at the University of Idaho. Professor Greg Möller, in the College of Agriculture and Life Sciences, along with engineers from the College of Engineering have teamed up to build the platform, and to further research the economical removal of phosphorus from various…
ApplicationApplication StoriesAutomation NotebookAutomationDirect SpotlightData CollectionIndustryIssue 28 - 2014Learning ResourcesNotebook IssuePLCProcess ControlProductProgrammable ControlSystem IntegratorsUser SolutionsWater/Wastewater
An Affordable Retrofit Prevents Expensive Replacements
The Harvest-Monrovia Water & Sewer Authority (HMWSA) was established in August 1965 to operate and maintain a water system to provide domestic water in the Harvest-Monrovia area of Madison County, located near Huntsville, Alabama. In the early years, the utility serviced only 700 customers. As a result of growth in the area, the HMWSA now…
ApplicationApplication StoriesAutomation NotebookData System MonitoringIndustryIssue 19 – 2011Learning ResourcesNotebook IssuePLCProductProgrammable ControlUser SolutionsWater/Wastewater
PLCs Give Wastewater Pumping Stations a Lift
Flexible, economical PLCs provide automatic failover, backup pump control, and remote lift station monitoring. The Moccasin Bend Wastewater Treatment Plant (WWTP) is part of the Interceptor Sewer System, which has served Chattanooga, Tennessee, and its surrounding metropolitan areas since it was built in 1952. The WWTP includes pumping stations as well as liquid and solids…
ApplicationApplication StoriesAutomation NotebookData CollectionIndustryIssue 16 – 2010Learning ResourcesNotebook IssuePLCProductProgrammable ControlWater/Wastewater
Evolution of the ChemFreePro® Ion Generator
In the 1960s, NASA conducted a research program to develop a small lightweight water purifier. The purifier was for use in the Apollo spacecraft, so low power usage and minimal maintenance were a must. The 9-ounce purifier, slightly larger than a cigarette pack and completely chlorine-free, was designed to dispense silver ions into the spacecraft’s…
ApplicationApplication StoriesAutomation NotebookDrivesHMIIndustryIssue 12 – 2008Learning ResourcesMachine ControlNotebook IssueOperator InterfacePLCProcess ControlProductProgrammable ControlUser SolutionsVariable Speed DrivesWater/Wastewater
AutomationDirect Products Help The Environment
Treating waste water generated in industrial plants requires an efficient, easy-to-use process which yields minimal by-product; it must be reliable and durable too. Environmental Compliance Equipment, in Palm City, Florida, designs systems to meet these requirements. One such system is marketed as ClearFlow. The ClearFlow System Explained ClearFlow systems can be integrated in almost any…
ApplicationApplication StoriesAutomation NotebookFeature StoryIndustryIssue 8 – 2007Learning ResourcesMachine ControlNotebook IssuePLCProcess ControlProductProgrammable ControlWater/Wastewater
Process Analyzer Uses WinPLC To Monitor Cyanide Destruction
NEXTChem Process Analyzers, LLC produces chemical process analyzers for industries such as metal treatment, metal finishing, chemical, wastewater, and pulp and paper. The analyzers automate laboratory measurements used for process control. Some of NEXTChem’s customers include a large aerospace company who uses the analyzer for measuring caustic cleaner for jet engine parts, and a major…