Linear Actuator OptionsLinear actuators, driven with servo or stepper motors, are an effective way to implement accurate automated machine motion. Linear actuators can also be driven by pneumatic or hydraulic methods, depending on the force, speed, accuracy, and cost requirements of an application. Electrically-driven actuators are the preferred solution for many applications, especially when automated…
Light-Operate or Dark-Operate Photoelectric Sensors. Which is Better for your Application?When choosing a photoelectric sensor for an application there are many things to consider. One of these considerations is whether to select a light-operate or dark-operate photoelectric sensor. The terms ?light-operate? and ?dark-operate? refer to when the sensor activates its output.Learn more Making a Clean…
Material Handling. Just like it sounds.Many components are involved in material handling systems, including motors, drives, sensors, pneumatics, controls, and safety products. When engineered properly, these components will work together in unison to efficiently move products, cases, or other materials from one location to another. Many things can go wrong or right depending on the…
Cybersecure and Remote-Friendly?Manufacturing companies recognize the need and value of practical remote access to their digital systems and data, but they also are aware of the associated cybersecurity risks. The NIST endorses ?defense-in-depth,? but what does this mean for OEMs, systems integrators, and end users looking to achieve workable and secure remote access?Learn more Select…
In-House Automation is the Key to CustomizationManufacturers are finding they can rapidly and flexibly adapt to changing production needs by engaging in-house personnel to deploy automation solutions.Automation is essential for improving productivity and quality, but many manufacturers serve markets where production volumes and product options vary drastically. Read more What is PID Control?PID is the most…
Robotic Beer Dispenser Hits the Ground Running?Reliable, rugged, and economical automation components are essential building blocks for bringing high-tech into consumer-facing applications.After working for more than a decade on industrial and automation projects, Grayson Dawson founded Hop Robotics to bring high-technology robotic serving systems to the food & beverage and hospitality sectors.Read more Free Practical…
Industrializing an Arduino: Making a Single-Board Controller Fit for the FactoryArduinos and similar devices can be highly versatile but are too delicate for industrial environments. So, the challenge for this project was to create an industrial type of application using an industrialized Arduino and associated components, to see what advantages they offer over conventional maker hardware. Read…
IO-Link is the Smart Choice for I/O ConnectivityA concept called the ?last mile problem? refers to the difficulty of completing the last link in a process, such as running internet cables to a user?s home. For industrial automation systems, one aspect of the last mile problem is connecting all the wiring from I/O modules to…
Cloud Connectivity Supports Smart HVACFor data centers powering the internet, the energy used to keep these systems cool is often the greatest operating cost, so small efficiency improvements can result in significant savings. IoT cloud connectivity lets experts effectively support increasingly complex HVAC systems, such as refrigerant-side economizers for data centers.Read more Old Reliable Just Got…
What is a VFD?A variable frequency drive (VFD) is an electronic device used to vary the frequency of an AC voltage to adjust the speed of an AC motor. VFDs also provide start and stop control, acceleration and deceleration, and overload protection. Many VFDs are networkable, allowing them to integrate into and provide feedback to…