“New! DURApulse GS20 Series High Performance AC Drives”… The DURApulse GS20 Series of next generation high-performance VFDs provide many standard and advanced functions in a compact reduced-size unit. The new GS20X series of AC drives is IP66/NEMA 4X rated for operation in harsh environments. AutomationDirect DURApulse GS20(X) drives start at $135.00 and have a two-year warranty. Watch…
“VFDs Expand Process Control Options”… Industrial process plant workers involved with motor controls back in the 1980s may remember them as huge electrical apparatuses, with rudimentary control capabilities.Today’s AC motor drives, occasionally called inverters but most commonly known as variable frequency drives (VFDs), are far more advanced and suitable for almost any application. Read more…
“CLICK PLC and C-more HMI Integral for Emergency Ventilator”… Using readily available AutomationDirect parts, an Auburn University team converted a CPAP machine to a high-functioning emergency ventilator in the midst of the COVID-19 pandemic. With the threat of ventilator shortages during the COVID-19 crisis, various organizations called on developers to build “emergency ventilators”. A team…
“VFDs Take Control”… Many industrial automation projects use programmable logic controllers (PLCs) for executing programs and variable frequency drives (VFDs) for running AC motors at commanded speeds. Some of the latest VFDs are actually hybrids with PLC-like programming functionality built right in, giving end users new options when designing automated systems. Read the article here…
“Can a Raspberry Pi Challenge a PLC?”… Single-board consumer microcontrollers are popular with hobbyists, but how do they stand up to industrial PLCs for more advanced process control applications? Many readers expressed considerable interest in a previous Control Design article comparing an Arduino microcontroller with a programmable logic controller (PLC) for basic flow control. This led author Doug…
Important Supply Update – Coronavirus Outbreak AutomationDirect is paying close attention to the fast-changing news regarding the Coronavirus. We are in close contact with all our suppliers to anticipate any potential effects on our supply chain as quickly as possible. We are also monitoring states’ mandates on any shipment/delivery restrictions we need to comply with….
AutomationDirect’s Food & Beverage Idea Book The Food and Beverage industry is a growing and changing field that’s becoming more and more reliant on automation and finding efficiencies. Click below to download our Food and Beverage eBook to see how big of a role automation plays. Topics Include: Top 10 Trends in the Industry NEMA…
New Industrial Grade Open-Source CPU The open-source Productivity®Open platform provides all the great features of a standard Arduino plus the added power and reliability of an industrial controller. The processor circuit of the P1AM-100 Arduino-compatible CPU is designed to mimic the Arduino MKRZero microcontroller. The P1AM-100 is compatible with most available Arduino MKR format shields, and/or…
Free HMI eBook AutomationDirect’s HMI Handbook delves into the world of human machine interfacing with informative chapters on selecting, designing and installing HMIs. But that’s just the first half, the back half of the book focuses specifically on C-more HMIs with chapters covering how to use screen objects, how to configure events, simulation basics, recipe…
16 Tips for an Effective HMI Do you have an HMI project coming up? Here are some helpful tips and guidelines for you to remember during your planning and implementation. A good starting point for HMI design is a text-based outline documenting each screen’s content. With the operator’s point-of-view and ease-of-use in mind, detail the…