AutomationDirect’s BRX PLC was announced as a Finalist in the Automation & Controls category for Plant Engineering’s 2017 Product of the Year. You can check out the new BRX PLC here. Winners will be announced on April 2, 2018.
AutomationDirect has added 206 new enclosures in 15 different categories to its Hubbell-Wiegmann line of metallic and non-metallic enclosures. New models include disconnect, pushbutton, padlocking, keylocking, floor-mount, freestanding and stainless steel enclosures, consoles/consolets, and enclosures with knockouts. Single-door freestanding enclosures with smaller removable hinge pins are now available. Multiple short hinge pins make it possible…
Still stuffed with turkey from Thanksgiving? Sit back and relax with the November issue of AutomationDirect’s newsletter! In this month’s issue check out a slideshare about IP69K ratings and download our free white paper about Automation Control System Specification, Design and Installation. After that, check out our other articles covering a range of topics such…
Starting at $98, two new 3-inch C-more Micro HMI panels are now available from AutomationDirect. C-more Micro panels display text, graphics, and bitmaps to effectively communicate critical HMI data to the operator.
AutomationDirect’s C-more EA9 series of touch screen HMIs now includes a 10-inch widescreen model and a 15-inch base model touch panel.
Congratulations to South Forsyth and Forsyth Central High Schools on their huge win at the Georgia Robotics Invitational Tournament and Showcase (aka “GRITS”) this past weekend.
Happy Halloween we have 2 treats this month , a contest and a giveaway! There’s an article on how to select the correct enclosure for your project. We have also included a SlideShare to help you select and size the right enclosure thermal management solution. Check out the newest application story on how Affinity Energy…
CLICK Series stackable micro brick PLCs are now available from AutomationDirect with both Ethernet communications capabilities and analog I/O built-in. 12 new units provide both discrete and analog I/O including four discrete inputs, four discrete outputs, two or four analog inputs and two analog outputs.
Remote access with cloud data logging options has been added to AutomationDirect’s line of industrial communications products. StrideLinx provides secure access over the “industrial internet” to remotely connect to monitor and troubleshoot multiple field devices. StrideLinx easily and affordably cloud enables any Ethernet-ready device.
The new Productivity1000 stackable micro PLC is the super compact yet highly capable member of AutomationDirect’s Productivity controller family. The P1000 is packed with many of the features of the Productivity series but housed in a smaller, slimmer design to provide space, budget and time savings.