AutomationDirect’s C-more CM5 HMI was announced as a Control Engineering 2024 Product of the Year nominee in the Control Systems category. Check out the link and cast your vote! Please note: You have to be a subscriber to CFE Media’s Control Engineering‘s eBook to cast a vote. The CM5 HMI series offers lower cost, high-performance HMIs in…
Every year, our local newspaper, Forsyth County News, conducts their Readers’ Choice “Best of Forsyth” contest to decide the favorite businesses, groups and professionals in Forsyth County amongst the community. The 2023 contest included 310 categories celebrated with 2,000 business nominations, 14,500 nominations and 336,000 votes from the community to select the winners. After being…
20:1 Scale Model of the 2022 FIRST Robotics 2022 Game Field provided by AutomationDirect.com AutomationDirect’s animation team converted the animation models into 3D printable models. This is the “playing field” for the FIRST Robotics Competition game for 2022. For more info about FIRST and the 2022 game: “RAPID REACT” – please visit the FIRST website. >>>…
AutomationDirect’s CLICK PLUS PLC, starting at just $89, is the next generation platform for basic control applications, building on reliable and familiar functionality, while adding advanced options like Wi-Fi and data logging. AutomationDirect’s CLICK PLUS PLC was announced as a Plant Engineering 2021 Product of the Year Finalist in the “Controls Systems” category. Check out…
AutomationDirect’s CLICK PLUS PLC, starting at just $89, is the next generation platform for basic control applications, building on reliable and familiar functionality, while adding advanced options like Wi-Fi and data logging. AutomationDirect’s CLICK PLUS PLC was announced as a Control Engineering 2022 Engineers’ Choice Awards Finalist in the “Controls Systems: PLCs, PACs” category. Check…
AutomationDirect’s ProductivityOpen PLC combines the IT-centric open-source capabilities of an Arduino-compatible controller with the robust reliability needed for industrial OT applications. AutomationDirect’s ProductivityOpen PLC was announced as a Control Engineering 2021 Engineers’ Choice Awards Honorable Mention winner in the Machine and Embedded Control – PLCs category. Check out the ProductivityOpen and see how specifying it…
The 2020 Digital Animation Award is offered to help encourage students to cultivate skills in design and creation of animation including, but not limited to, storytelling, creativity, use of computer software, and an understanding of different techniques and forms of animation. This award is open to all FIRST Robotics Competition teams.
AttaBox NewSentry series thermoplastic PVC (Polyvinyl Chloride) junction boxes are extremely rugged and light enclosures for harsh, aggressive environments and are well-suited for extremely wet and corrosive environments. Uses vary from high-end electronics to extreme corrosive applications both indoors and out, and their small footprint allows use in tight spaces. The easily workable PVC construction…
Automation professionals have voted for the AutomationDirect family of operator interface hardware and software, once again making them a top choice for their applications. AutomationDirect operator interface (OI) hardware and software were recently recognized in Control Design 2019 Readers’ Choice Awards. This awards program invites readers with buying influence or authority to vote by writing…
AutomationDirect’s Productivity1000 PLC was selected for its ability to provide cost-effective control of machines and processes. AutomationDirect’s Productivity1000 PLC was announced as a Plant Engineering 2018 Engineers’ Choice Awards Bronze Winner for the Automation & Control category. You can find more info on the Productivity1000 PLC here and explore if it would be a good…