The decision to purchase a high-performance power supply is often a balancing act between upfront costs and long-term benefits. While standard power supplies may be sufficient for basic operations, high-performance models offer a range of advanced features designed to enhance efficiency, reliability, and overall system performance. While the initial expense may be higher, it is…
There are many practical and cost-effective ways for designers to incorporate automation redundancy for systems of any size. Automation redundancy has largely been reserved for larger process automation systems due to cost and complexity. However, there are now more products and design strategies suitable for applying redundancy to smaller-scale systems. Rin Irvin at AutomationDirect covers…
ApplicationCircuit ProtectionElectrical PowerFood and BeverageProcess ControlProductRelays & TimersTerminal Blocks & Wiring
Robotic Beer Dispenser Hits the Ground Running
Reliable, rugged, and economical automation components are essential building blocks for bringing high-tech into consumer-facing applications. After working for more than a decade on industrial and automation projects, Grayson Dawson founded Hop Robotics to bring high-technology robotic serving systems to the food & beverage and hospitality sectors. He wrote a success story article that ran…
Electrical power products provide safe and efficient power services for industrial and commercial use, from incoming facility power to endpoint distribution and filtering. AutomationDirect provides a variety of electrical power products for all of your needs! Download our Guide to Power Products here! This Download Includes: DC Power Supplies Transformers Power and Process Monitoring And…
What is Needed for Industrial Control Panels? Industrial control panels are fundamental for protecting electrical, instrumentation, and control devices. The AutomationDirect portfolio of enclosures and components can help users obtain everything they need to create control panel solutions. Industrial control panels are commonly used for distributing power, housing pneumatics, and protecting automation electronics associated with…
We’ve all experienced issues with interference of Wi-Fi signals whether on our phones or computers. Sometimes the Wi-Fi goes out or we can’t update our connection and it causes an error. This is undoubtedly annoying but nothing compared to the interference that electrical noise can produce in certain situations. This kind of interference can actually…
Transformers to the rescue! No, not the kind of “transformers” made famous by Hasbro™ and Hollywood. These transformers manufactured by Hammond Power Solutions came to the rescue of the much-loved Canadian event known as the Calgary Stampede after massive flooding in 2013 brought the city to a standstill and threatened to cancel the event that…
+Tech TopicsAutomation NotebookElectrical PowerIssue 16 – 2010Learning ResourcesNotebook IssueProductTechnology Brief
Transformers: Application, Construction and Efficiencies (Part 2)
The Conclusion of a Two-Part series In the last issue of NOTEBOOK, we discussed the two categories of transformers commonly available and typical applications for them. The final category is control transformers, which are commonly incorporated into a machine element. This is the broadest category, as voltage matching situations will almost certainly be encountered which, in…
+Tech TopicsAutomation NotebookElectrical PowerIssue 15 – 2009Learning ResourcesNotebook IssueProductTechnology Brief
Transformers: Application, Construction and Efficiencies
Part One of a Two-Part Series Although most of us have encountered transformers in our professional lives, it’s surprising just how little the average designer or technician knows about them. A transformer’s principal function is to “transform” alternating current from an undesirable voltage to a voltage that is appropriate for the circuit at hand. A…
+Tech TopicsAutomation NotebookElectrical PowerEnergy/UtilitiesIndustryIssue 6 – 2006Learning ResourcesNotebook IssueProductTechnology Brief
Dealing with Low-voltage Power Issues
Voltage Dip and Power Failure Voltage dip and power failure – these are two events that can cause everything in a manufacturing and processing facility to go dim. When a machine or processing line goes down due to a power failure, it can cost a company thousands of dollars in as little as an hour….