Unshackling Industrial Data Access
Operator InterfaceProductProgrammable Control

Unshackling Industrial Data Access

Modern PLCs and HMIs make it easy to implement extensive data connectivity and analytics. By: Damon Purvis, AutomationDirect Modern consumers are increasingly familiar with tailored experiences, abundant information, and generally getting things “their way.” Those working in the industrial manufacturing and automation sectors, on the other hand, have not always enjoyed such flexibility. Fortunately, hardware…
Automating a Luxury Bus
Application StoriesDistribution/LogisticsHMIIndustryOperator InterfacePLCProductProgrammable Control

Automating a Luxury Bus

Industrial automation products are useful for much more than traditional applications, as PLCs and HMIs can be used in all sorts of unique commercial markets. Byline: Mark McHenry, Systems & Controls Other than being large and generally rectangular-shaped, a modern custom bus—the type frequented by touring music stars, mobile multi-millionaires, and campaigning politicians—bears little resemblance…
Turning Up the Heat on a Balky Boiler
Application StoriesHMIOperator InterfacePLCProductProgrammable Control

Turning Up the Heat on a Balky Boiler

Applying commercial off-the-shelf automation products can provide the most capable and supportable solution for end users trapped with underperforming automation systems, as with this application. By: Aaron Stahl and Edward Stahl, Spring Valley Electric Worldwide, there are countless examples of businesses forced to work inefficiently because they are using equipment which is automated by systems…
Automating Escape Room Experiences
Application StoriesHMIOperator InterfacePLCProductProgrammable Control

Automating Escape Room Experiences

Industrial automation products can also be applied to unique applications, like the advanced control needed for a sophisticated escape room. Escape rooms are immersive adventure games where players solve puzzles to break out from a themed environment within a set time. While seemingly unrelated to industrial automation, a systems integrator (SI) leveraged expertise gained from…
What is an HMI?
Operator InterfaceProduct

What is an HMI?

A digital graphical human-machine interface is usually the best way for users to interact with any type of monitoring or control system, and industrial versions are specially designed to withstand challenging environments. For practically every type of machinery or equipment ever put into service, there has been a need for some type of operator interface…
The Evolution of the Human Machine Interface
Issue 52, 2024Notebook IssueOperator InterfaceProduct

The Evolution of the Human Machine Interface

From high resolution graphics to more interconnectivity and mobility, the HMI has become instrumental to plant productivity. Around 40 years ago, operator interfaces on the factory floor consisted of manual push buttons, switches, and dials. More sophisticated versions might incorporate a few indicator lights that could flash or change color to communicate alerts sent by…
Installing a Rock-Solid Automation Retrofit
Application StoriesHMIOperator InterfacePLCProductProgrammable Control

Installing a Rock-Solid Automation Retrofit

This electrical contractor relied on AutomationDirect PLC and HMI hardware and software to rapidly rip-and-replace the controls on a failing rock crusher. Equipment used in rock quarrying operations is subjected to extremes of dirt, vibration, heat, and more, pressing mechanical and electrical systems to the limit. When the crushing equipment legacy automation at one site…
Mining Sunbeams – Solar Thermal Leverages the Sun for Producing Heat Energy
Application StoriesHMIOperator InterfacePLCProductProgrammable Control

Mining Sunbeams – Solar Thermal Leverages the Sun for Producing Heat Energy

Solar thermal installations need advanced control systems to optimize energy harvesting, storage, and distribution at remote mining operations. For certain applications in the right geographic areas, solar thermal can be a cost effective and low carbon way to supply large-scale heat energy. Flemming Jørgensen, of Jorgensen Thermal solutions, supplies these systems, and he needed to…
Redundancy Options for Smaller Automation Systems
Electrical PowerOperator InterfaceProcess Sensing & ControlProductProgrammable Control

Redundancy Options for Smaller Automation Systems

There are many practical and cost-effective ways for designers to incorporate automation redundancy for systems of any size. Automation redundancy has largely been reserved for larger process automation systems due to cost and complexity. However, there are now more products and design strategies suitable for applying redundancy to smaller-scale systems. Rin Irvin at AutomationDirect covers…