Pneumatics have been used in industrial machines and manufacturing plants and facilities for decades, so most of the basic components are tried and true, with significant innovations few and far between. But there are many innovative ways to combine these different components to create pneumatic subsystems. The explains four pneumatic subsystems, showing how combining basic…
The maintenance department at Blank Park Zoo (www.blankparkzoo.com) in Des Moines, Iowa was looking for a cost-effective way to keep their train running safely. The train ride is part of the 49-acre park which includes almost 1500 animal specimens.
ApplicationApplication StoriesEducation/DIYEntertainmentHMIIndustryMachine ControlOnline OnlyOperator InterfacePLCPneumaticsPneumaticsProductProgrammable ControlVariable Speed Drives
The Halloween Box
In every haunted house, you’ll find automated props: chairs that rock on their own, slamming doors, rattling chains, drawers opening and closing as if by some supernatural force. These “tricks” enhance the “treat” of getting the life scared out of you. The process behind making a Halloween prop can be quite simple. Here is just…
ApplicationApplication StoriesAutomation NotebookeBookIndustryIssue 34 - 2016Learning ResourcesManufacturingMaterial HandlingNotebook IssueOnline OnlyPackagingPLCPneumaticsProductProgrammable ControlSimple PLCUser Solutions
CLICK PLCs and Pneumatics Team Up for Success at Ridgeline Machine
Ridgeline Machine made extensive use of pneumatics when building a low-cost, small-footprint, portable traymaker to replace a manual process for one of their customers. Ridgeline Machine Design, LLC (RMD), founded in 2012, is primarily a packaging machinery producer, and the company’s owners have over 40 years experience designing and building custom machinery. RMD builds packaging…
Check out this Q&A about all things pneumatic cylinders! Q. What pneumatic cylinders and accessories are available from AutomationDirect? A. The NITRA A-Series non-repairable stainless steel round body cylinders includes bore sizes from 7/16” to 2” and stroke lengths from 1/2” to 18” to meet a broad range of applications. These high quality cylinders are…