Here are some best practices to supply safe, clean and dry air to a machine or an item of equipment. Pat Phillips, Product Manager, Fluid Power & Mechanical Products at AutomationDirect, wrote an article for the October 2018 issue of Fluid Power World magazine titled What type of air prep is required for plant compressed air?…
ApplicationApplication StoriesAutomationDirect SpotlightFacilitiesIndustryIssue 41 - 2019Notebook IssuePLCProcess ControlProductProgrammable ControlSystem Integrators
Open System Provides Precise Temperature Control
System integrator Affinity Energy worked with the University of North Carolina at Chapel Hill to design and install a new temperature control system for their research chambers. By Allan Evora, President of Affinity Energy The University of North Carolina (UNC) at Chapel Hill was spending too much time and money supporting an existing control system….
ApplicationApplication StoriesEnergy/UtilitiesFacilitiesHMIIndustryLearning ResourcesOnline BlogOnline OnlyPLCProcess Control
System Integrator and AutomationDirect partner Affinity Energy Designed, Built and Installed a Research Chamber Temperature Control System
The University of North Carolina (UNC) at Chapel Hill spends almost $1 billion on research annually, ranking eighth among universities in the U.S. However, it was spending too much money and time supporting an existing temperature chamber control system.
Drive or motor failures, lights flickering, analog signal variations and poor encoder count repeatability are all symptoms of electrical noise issues. Automated machinery is often the victim of electrical noise, and frequently also the source. Whether it’s electromagnetic interference (EMI) or radio frequency interference (RFI), there are many options available to reduce its effects. Both…
+Tech TopicsApplicationeBookeBook Landing PagesFacilitiesIndustryLearning ResourcesMachine ControlOnline Only
Machine Maintenance Checklist
It is important to develop a routine maintenance schedule for your automated control system. Having a routine schedule for checking critical components and devices in the system will increase the longevity of the system and more importantly, it will help reduce future problems. Set up the schedule based on a monthly or quarterly time period,…
ApplicationApplication StoriesAutomation NotebookData System MonitoringEducation/DIYFacilitiesIndustryIssue 27 – 2013Learning ResourcesNotebook IssueOperator InterfacePLCProductProgrammable ControlStudent SpotlightTest and Measurement
Students help Manufacturing Center See AND Do More
When the mechatronics students at Catawba Valley Community College (CVCC) in Hickory, North Carolina, went looking for a suitable project to challenge their recently acquired PLC and HMI skills, they didn’t have to go far. The Problem The college’s Manufacturing Solutions Center (MSC) in nearby Conover needed a way to monitor the status of a…
+Tech TopicsApplicationApplication StoriesAutomation NotebookCover StoriesEnergy/UtilitiesFacilitiesIndustryIssue 24 - 2012Learning ResourcesManufacturingNotebook IssuePLCProcess ControlProductProgrammable Control
Reducing Total Cost of Ownership
Automation is a key component when developing strategies to help customers reduce their operating costs. Many times when making buying decisions, people look only at the initial price of an item without considering other factors that contribute to the overall cost of owning that product. For example, a certain laptop may seem like a great…
ApplicationApplication StoriesAutomation NotebookAutomationDirect SpotlightFacilitiesIndustryIssue 17 – 2010Learning ResourcesNotebook IssueOperator InterfacePLCProcess ControlProductProgrammable ControlSystem IntegratorsUser Solutions
Volatile Material Handling for IBM
When IBM needed a control and delivery system for Silane gas at the T. J. Watson Research Facility in Yorktown Heights, NY, they turned to KCC Software of Huntsville, AL. Managing Silane Gas Silane gas is essential in an ultra-pure method of applying silicon in the manufacturing of semiconductors and solar panels. The SiH4 compound,…
ApplicationApplication StoriesAutomation NotebookFacilitiesFeature StoryIndustryIssue 9 – 2007Learning ResourcesMachine ControlNotebook IssuePLCProductProgrammable ControlSecurity
Anti-Terrorist Barriers Help Protect Facilities
Since the terrorist attacks of September 11, 2001, the need for perimeter security of potentially threatened facilities has increased dramatically. To accomplish this, several facilities around the globe have been installing devices called anti-terrorist barriers, used as added protection against invasion of potentially dangerous vehicles. Domestically, these anti-terrorist devices can be found at Federal Reserve…
ApplicationApplication StoriesAutomation NotebookEnergy/UtilitiesFacilitiesIndustryIssue 3 – 2005Learning ResourcesNotebook IssuePLCProcess ControlProductProgrammable ControlUser Solutions
Controlling Nature's Way of Cooling
When conventional air conditioning systems were no longer adequate to cool General Tool Company’s (GTC) facility in Cincinnati, OH, the company began looking for an alternative solution. A roof mist sprinkling system from Sprinkool™ Systems International, Inc. in Killen, AL, would provide evaporative cooling of the roof and ceiling zone of the plant to reduce…