Content CollectionsUncategorized

Equipment Safety | Protect More Than Just Your Equipment with AutomationDirect

No matter what industry you’re in, there is always electrical/electronic enclosures and cabinets along with the machinery and other ancillary equipment that independently or together contribute to complete a process efficiently. Some of this equipment is designed to run automatically controlled by a PLC and other automation equipment depending on existing conditions in a production line or process. Other equipment requires occasional and sometimes constant intervention from a human operator. Equipment failure or malfunction protection is very important to prevent harm to operators, reduce costs to replace damaged equipment/devices, and prevent losses from production delay costs.

Investing in the right safety equipment and devices will more than pay for itself by protecting personnel, prolonging equipment life, and reducing costly down-time. These big savings are even more noticeable when you find the right equipment at the best price while also saving in other costs like technical support, shipping costs, fast delivery, warranties and more. This is why AutomationDirect works so hard to provide the best prices in the industry for the best quality products, along with award-winning FREE technical support, a vast library of training videos and documentation, the best customer service in the industry, FREE and FAST 2-day shipping for orders $49 and over, and 30-day money-back guarantee on practically every product we sell. Go ahead, we invite you to check out our videos, blogs, documentation and more for our enclosures, pilot devices, safety switches, circuit and surge protection devices, and so many more products that help you protect your equipment and personnel.

Looking for even more content? Click on our Product tab to see more articles on equipment safety!


Circuit ProtectionEquipment SafetyOnline OnlyProduct

Industrial Surge Protection: Why Use Mersen Surge Protection Devices?

Most of us have a basic idea of what power surge means. We know it is something that affects the electric power we receive and that it can cause serious damage to industrial equipment, computers, and sensitive electronics. To offer a simple definition, a power surge is a fluctuation of the voltage coming in through…
Control & Signaling DevicesEquipment SafetyOnline OnlyProduct

Patlite Stack Lights: Stacked Above the Rest

I remember years ago walking into a production facility and being intrigued by the processes taking place in each section of the production line. It was so interesting to see how things were shaped, packed, filled and more. Every step or section of the production line had a specific purpose that needed to be completed…
+Tech TopicsAutomation NotebookEnclosures & AccessoriesEquipment SafetyIssue 26 – 2013Learning ResourcesNotebook IssueProductTechnology Brief

What to Know When Selecting an Enclosure

NEMA enclosures house all kinds of electrical components from simple terminal blocks, to industrial automation systems, to high voltage switchgear. In industrial automation systems, NEMA enclosures often house motor controls, drives, PLC/PC control systems, pushbuttons, and termination systems. Some enclosures are shaped to be operator consoles. AutomationDirect offers over 2,200 enclosure part numbers across NEMA…
Equipment SafetyLearning ResourcesOnline BlogOnline OnlySafety

Emergency Stop Control Stations: One Push Can Save Your Life

Let’s take a minute to think about how far we have advanced with innovation and technology. It is truly amazing when you look at the devices and products we develop these days. From a simple small piece of wood with a spring-loaded thin u-shaped metal rod and an extremely simple trigger mechanism designed to reduce…
Equipment SafetyLearning ResourcesOnline BlogOnline Only

Everything You Need to Know About Ferrules: A Comprehensive Guide

What is a Ferrule? What is a Ferrule? I ask myself this question thinking specifically of the small metal tube with a colored insulated plastic end where you can insert wire strands and crimp the tube securely to the wire. To answer this question, I decided to do an internet search to see what I…
+Tech TopicsCircuit ProtectionEquipment SafetyLearning ResourcesOnline OnlyProduct

What Type of Circuit Protection Do I Need?

Circuit Protection is a big topic. With so many types of products available, coupled with the fact that I think I am getting old, I have found that it is becoming increasingly difficult to keep it all straight. If you share in this frustration, no worries because conveniently located below is a chart that I think might…
Equipment SafetyProductSafety

Consider Newer Electrical Safety Products and Technologies

Designers can improve personnel safety by incorporating modern products and technologies, and by following a “design for safety” approach. Marty Kronz at AutomationDirect wrote an article for the February 2023 issue of Applied Automation. Titled Addressing Electrical Safety Hazards, this article identifies how some newer products, sometimes in combination with automation, can increase the effectiveness…
Enclosures & AccessoriesEquipment SafetyOnline OnlyProduct

Enclosure Thermal Management: Product Types and Selection Overview

Industrial facilities use many electrical enclosures to house automation and electrical components. Several of these enclosures require cooling and/or heating to control the climate within the enclosure to prevent condensation or component overheating. In this SlideShare, you will learn about the different types of climate control, reasons for use, and how to select and size…
Equipment SafetyFood and BeverageFood Beverage AutomationIndustryLearning ResourcesOnline BlogOnline Only

What is IP69K?

IP69K Definition IP69K is a product standard rating developed to ensure that products carrying this rating comply with required simulated environmental conditions. The most common areas requiring IP69K devices are areas where heavy washdowns are required. Therefore, IP69K rated devices are a must to prevent damage to electronic devices and instrumentation during the washdown procedures….
Content CollectionsEquipment SafetyProductSafetySafety Common Sense

Safety, Prevent Accidents with Proper Planning

It can happen at the best workplaces and in the safest environments but it’s always chilling news when you come into work and hear that there has been a workplace injury. Whether you are in charge of safety, are a production manager, or are a plant manager, so many questions go through your mind at…
Equipment SafetyLearning ResourcesOnline BlogOnline Only

Every Motor Deserves a Quality Liquid-Tight Conduit

You get a call from the production floor because a machine is not running right. You go check it and find out that the motor is acting up, has corrosion damage inside the junction box, which is probably also contributing to the imminent death of the motor. Now you need to replace it but don’t…
AC Motors and ControlsEquipment SafetyLearning ResourcesMotor ControlsOnline BlogOnline OnlyProduct

AC Motor On/Off Controls | Automation Notes

Most control systems have to make things move, and that usually involves motors. Lifting, pumping, robotics, conveyors, fans – pretty much everything uses a motor of some kind. General purpose one- or three-phase AC motors are great for simple on/off systems; Inverter-duty motors are specifically designed for operation with variable frequency drives or VFDs. General…